<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: s32k116 The Stop2 low power mode cannot be woken up with a CAN message in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/s32k116-The-Stop2-low-power-mode-cannot-be-woken-up-with-a-CAN/m-p/1094951#M8427</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Zheng,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the CAN module to be able to wake up the MCU, it needs to be in&amp;nbsp;Pretended Network mode, for more information about the PNET mode please check the section 55.5.5 Receive process under Pretended Networking mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if you are using any STOP mode I will not suggest using to connect an external debugger, if you are using the debugger is possible that the Low Power Mode is not called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Aug 2020 16:09:48 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2020-08-18T16:09:48Z</dc:date>
    <item>
      <title>s32k116 The Stop2 low power mode cannot be woken up with a CAN message</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/s32k116-The-Stop2-low-power-mode-cannot-be-woken-up-with-a-CAN/m-p/1094950#M8426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" data-group="0-0" data-section="0" data-sentence="0" style="color: #333333; background-color: #f7f8fa; font-weight: normal; font-size: 14px;"&gt;Referring to the sample code provided by the official, CAN configure PE clock source to; PE clock source is 8MHz; it cannot be awakened in Jlink mode.&lt;/SPAN&gt;&lt;SPAN class="" data-group="0-1" data-section="0" data-sentence="1" style="color: #333333; background-color: #f7f8fa; font-weight: normal; font-size: 14px;"&gt;PE clock source is configured as Peripheral clock, and the PE clock is 48MHz. It can be normally awakened during JLink debugging. However, after taking down JLink to run the connection can and sending a message to MCU to STOP2 mode, it cannot be awakened by sending another message.&lt;/SPAN&gt;&lt;SPAN class="" data-group="0-2" data-section="0" data-sentence="2" style="color: #333333; background-color: #f7f8fa; font-weight: normal; font-size: 14px;"&gt;Please help me, thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Aug 2020 07:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/s32k116-The-Stop2-low-power-mode-cannot-be-woken-up-with-a-CAN/m-p/1094950#M8426</guid>
      <dc:creator>972276616</dc:creator>
      <dc:date>2020-08-14T07:11:49Z</dc:date>
    </item>
    <item>
      <title>Re: s32k116 The Stop2 low power mode cannot be woken up with a CAN message</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/s32k116-The-Stop2-low-power-mode-cannot-be-woken-up-with-a-CAN/m-p/1094951#M8427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Zheng,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the CAN module to be able to wake up the MCU, it needs to be in&amp;nbsp;Pretended Network mode, for more information about the PNET mode please check the section 55.5.5 Receive process under Pretended Networking mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if you are using any STOP mode I will not suggest using to connect an external debugger, if you are using the debugger is possible that the Low Power Mode is not called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2020 16:09:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/s32k116-The-Stop2-low-power-mode-cannot-be-woken-up-with-a-CAN/m-p/1094951#M8427</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-08-18T16:09:48Z</dc:date>
    </item>
  </channel>
</rss>