<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックConfig PTIL_PTIL1 as input</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Config-PTIL-PTIL1-as-input/m-p/1087090#M8392</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need help with the config of PortL by the 12ZVCA192 with 48 Pins&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will use the PTIL_PTIL1 as normal digital input. but it dosent work. i have always a low on this pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This input detec a resistor. it is set, the pins is on low. with out it shuod detec a high over intern pullup&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but nothing chance when i switch the Polaity select from Pulldown to pullup in CodeWarrior Hardware selektion&lt;/P&gt;&lt;P&gt;i set it to digital Input&lt;/P&gt;&lt;P&gt;what can i do ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 11 Apr 2020 13:53:03 GMT</pubDate>
    <dc:creator>nxp14</dc:creator>
    <dc:date>2020-04-11T13:53:03Z</dc:date>
    <item>
      <title>Config PTIL_PTIL1 as input</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Config-PTIL-PTIL1-as-input/m-p/1087090#M8392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need help with the config of PortL by the 12ZVCA192 with 48 Pins&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will use the PTIL_PTIL1 as normal digital input. but it dosent work. i have always a low on this pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This input detec a resistor. it is set, the pins is on low. with out it shuod detec a high over intern pullup&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but nothing chance when i switch the Polaity select from Pulldown to pullup in CodeWarrior Hardware selektion&lt;/P&gt;&lt;P&gt;i set it to digital Input&lt;/P&gt;&lt;P&gt;what can i do ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Apr 2020 13:53:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Config-PTIL-PTIL1-as-input/m-p/1087090#M8392</guid>
      <dc:creator>nxp14</dc:creator>
      <dc:date>2020-04-11T13:53:03Z</dc:date>
    </item>
    <item>
      <title>Re: Config PTIL_PTIL1 as input</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Config-PTIL-PTIL1-as-input/m-p/1087091#M8393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to recommend to look at the section "2.5.5 Open Input Detection&amp;nbsp;&lt;SPAN&gt;on PL[1:0] (HVI)"&lt;/SPAN&gt;&amp;nbsp;and "Figure 2-36. Digital Input Read with Pullup Enabled" in RM rev 12.1. Also, please, check if registers are correctly set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2020 09:20:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Config-PTIL-PTIL1-as-input/m-p/1087091#M8393</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2020-04-15T09:20:52Z</dc:date>
    </item>
  </channel>
</rss>