<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CW 10: Controlling Link Order in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-10-Controlling-Link-Order/m-p/1061151#M8308</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any way to control the link order in CodeWarrior 10.4 for HCS08 micros?&amp;nbsp; There's buzz about a "Link Order tab" but that seems to be limited to ARM, et al.&amp;nbsp; The only way I can control the link order is to disable "Generate Makefiles automatically" in project-&amp;gt;properties-&amp;gt;C/C++Build then manually shuffle the file list in the &amp;lt;project&amp;gt;.args file.&amp;nbsp; Seems like there ought to be a more simple way ('cause I'll forget I've disabled makefile generation and have all sorts of contortions later on).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any pointers!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Jun 2020 19:59:15 GMT</pubDate>
    <dc:creator>dougpaulsen</dc:creator>
    <dc:date>2020-06-04T19:59:15Z</dc:date>
    <item>
      <title>CW 10: Controlling Link Order</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-10-Controlling-Link-Order/m-p/1061151#M8308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any way to control the link order in CodeWarrior 10.4 for HCS08 micros?&amp;nbsp; There's buzz about a "Link Order tab" but that seems to be limited to ARM, et al.&amp;nbsp; The only way I can control the link order is to disable "Generate Makefiles automatically" in project-&amp;gt;properties-&amp;gt;C/C++Build then manually shuffle the file list in the &amp;lt;project&amp;gt;.args file.&amp;nbsp; Seems like there ought to be a more simple way ('cause I'll forget I've disabled makefile generation and have all sorts of contortions later on).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any pointers!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 19:59:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-10-Controlling-Link-Order/m-p/1061151#M8308</guid>
      <dc:creator>dougpaulsen</dc:creator>
      <dc:date>2020-06-04T19:59:15Z</dc:date>
    </item>
    <item>
      <title>Re: CW 10: Controlling Link Order</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-10-Controlling-Link-Order/m-p/1061152#M8309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Doug,&lt;/P&gt;&lt;P&gt;There is no option in CW10.4 for HCS08 to change link order&amp;nbsp;&lt;/P&gt;&lt;P&gt;Your method is the exact method to&amp;nbsp;do it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2020 03:34:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-10-Controlling-Link-Order/m-p/1061152#M8309</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-06-05T03:34:18Z</dc:date>
    </item>
  </channel>
</rss>