<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Error -1073741811 in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-1073741811/m-p/1059115#M8303</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Tony,&lt;/P&gt;&lt;P&gt;I have just created a new project based on MC56F8013, I have tried to compile it, it is okay.&lt;/P&gt;&lt;P&gt;This is the compiling/linking inf on the Console menu of CW tools:&lt;/P&gt;&lt;P&gt;If you new a project based on MC56F8013, then compile/link it on IDE of CW tools, what is the result?&lt;/P&gt;&lt;P&gt;BTW, did you compile an old project or new project?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;**** Clean-only build of configuration FLASH_SDM for project test_8013 ****&lt;BR /&gt;Build complete for project test_8013&lt;/P&gt;&lt;P&gt;**** Build of configuration FLASH_SDM for project test_8013 ****&lt;/P&gt;&lt;P&gt;"C:\\Freescale\\CW MCU v11.1\\gnu\\bin\\mingw32-make" -j8 all &lt;BR /&gt;'Building file: ../Sources/Events.c'&lt;BR /&gt;'Building file: ../Sources/main.c'&lt;BR /&gt;'Building file: ../Project_Settings/Startup_Code/56F80xx_init.asm'&lt;BR /&gt;'Building file: ../Generated_Code/Cpu.c'&lt;BR /&gt;'Building file: ../Generated_Code/Vectors.c'&lt;BR /&gt;'Executing target #1 ../Sources/Events.c'&lt;BR /&gt;'Executing target #2 ../Sources/main.c'&lt;BR /&gt;'Executing target #3 ../Project_Settings/Startup_Code/56F80xx_init.asm'&lt;BR /&gt;'Executing target #4 ../Generated_Code/Cpu.c'&lt;BR /&gt;'Executing target #5 ../Generated_Code/Vectors.c'&lt;BR /&gt;'Invoking: DSC Compiler'&lt;BR /&gt;'Invoking: DSC Compiler'&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e" -c @@"Sources/Events.args" -o "Sources/Events_c.obj" "../Sources/Events.c" -MD -gccdep&lt;BR /&gt;'Invoking: DSC Assembler'&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e" -c @@"Sources/main.args" -o "Sources/main_c.obj" "../Sources/main.c" -MD -gccdep&lt;BR /&gt;'Invoking: DSC Compiler'&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwasm56800e" @@"Project_Settings/Startup_Code/56F80xx_init.args" -o "Project_Settings/Startup_Code/56F80xx_init_asm.obj" "../Project_Settings/Startup_Code/56F80xx_init.asm" -MD -gccdep&lt;BR /&gt;'Invoking: DSC Compiler'&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e" -c @@"Generated_Code/Cpu.args" -o "Generated_Code/Cpu_c.obj" "../Generated_Code/Cpu.c" -MD -gccdep&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e" -c @@"Generated_Code/Vectors.args" -o "Generated_Code/Vectors_c.obj" "../Generated_Code/Vectors.c" -MD -gccdep&lt;BR /&gt;'Finished building: ../Project_Settings/Startup_Code/56F80xx_init.asm'&lt;BR /&gt;' '&lt;BR /&gt;'Finished building: ../Sources/Events.c'&lt;BR /&gt;'Finished building: ../Sources/main.c'&lt;BR /&gt;'Finished building: ../Generated_Code/Cpu.c'&lt;BR /&gt;'Finished building: ../Generated_Code/Vectors.c'&lt;BR /&gt;' '&lt;BR /&gt;' '&lt;BR /&gt;' '&lt;BR /&gt;' '&lt;BR /&gt;'Building target: test_8013.elf'&lt;BR /&gt;'Executing target #6 test_8013.elf'&lt;BR /&gt;'Invoking: DSC Linker'&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwld56800e" -o "test_8013.elf" @@"test_8013.args"&amp;nbsp; &lt;BR /&gt;C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwld56800e|Linker|Warning&lt;BR /&gt;&amp;gt;Overlap of the .interrupt_vectorsboot section and .interrupt_vectors section.&lt;BR /&gt;C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwld56800e|Linker|Warning&lt;BR /&gt;&amp;gt;Overlap of the .interrupt_vectors section and .interrupt_vectorsboot section.&lt;BR /&gt;C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwld56800e|Linker|Warning&lt;BR /&gt;&amp;gt;Binary flash image: P address overlaps with something at word address 0x0&lt;BR /&gt;'Finished building target: test_8013.elf'&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Jun 2020 02:24:00 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2020-06-09T02:24:00Z</dc:date>
    <item>
      <title>Error -1073741811</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-1073741811/m-p/1059114#M8302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have installed code warrior 11.1, update 1 and 2. after compiling the project have &lt;SPAN&gt;Error -1073741811&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;i am using windows10.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;**** Clean-only build of configuration FLASH_SDM for project sin20200 ****&lt;BR /&gt;Build complete for project sin20200&lt;/P&gt;&lt;P&gt;**** Build of configuration FLASH_SDM for project sin20200 ****&lt;/P&gt;&lt;P&gt;"C:\\Freescale\\CW MCU v11.1\\gnu\\bin\\mingw32-make" -j8 all &lt;BR /&gt;'Building file: ../Sources/Events.c'&lt;BR /&gt;'Building file: ../Sources/main.c'&lt;BR /&gt;'Building file: ../Project_Settings/Startup_Code/56F80xx_init.asm'&lt;BR /&gt;'Building file: ../Generated_Code/Cpu.c'&lt;BR /&gt;'Building file: ../Generated_Code/Vectors.c'&lt;BR /&gt;'Executing target #1 ../Sources/Events.c'&lt;BR /&gt;'Executing target #2 ../Sources/main.c'&lt;BR /&gt;'Executing target #3 ../Project_Settings/Startup_Code/56F80xx_init.asm'&lt;BR /&gt;'Executing target #4 ../Generated_Code/Cpu.c'&lt;BR /&gt;'Executing target #5 ../Generated_Code/Vectors.c'&lt;BR /&gt;'Invoking: DSC Compiler'&lt;BR /&gt;'Invoking: DSC Compiler'&lt;BR /&gt;'Invoking: DSC Assembler'&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e" -c @@"Sources/main.args" -o "Sources/main_c.obj" "../Sources/main.c" -MD -gccdep&lt;BR /&gt;'Invoking: DSC Compiler'&lt;BR /&gt;'Invoking: DSC Compiler'&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e" -c @@"Sources/Events.args" -o "Sources/Events_c.obj" "../Sources/Events.c" -MD -gccdep&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwasm56800e" @@"Project_Settings/Startup_Code/56F80xx_init.args" -o "Project_Settings/Startup_Code/56F80xx_init_asm.obj" "../Project_Settings/Startup_Code/56F80xx_init.asm" -MD -gccdep&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e" -c @@"Generated_Code/Cpu.args" -o "Generated_Code/Cpu_c.obj" "../Generated_Code/Cpu.c" -MD -gccdep&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e" -c @@"Generated_Code/Vectors.args" -o "Generated_Code/Vectors_c.obj" "../Generated_Code/Vectors.c" -MD -gccdep&lt;BR /&gt;'Finished building: ../Project_Settings/Startup_Code/56F80xx_init.asm'&lt;BR /&gt;'Finished building: ../Sources/main.c'&lt;BR /&gt;'Finished building: ../Sources/Events.c'&lt;BR /&gt;'Finished building: ../Generated_Code/Cpu.c'&lt;BR /&gt;' '&lt;BR /&gt;'Finished building: ../Generated_Code/Vectors.c'&lt;BR /&gt;' '&lt;BR /&gt;' '&lt;BR /&gt;' '&lt;BR /&gt;' '&lt;BR /&gt;'Building target: sin20200.elf'&lt;BR /&gt;'Executing target #6 sin20200.elf'&lt;BR /&gt;'Invoking: DSC Linker'&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwld56800e" -o "sin20200.elf" @@"sin20200.args" &lt;BR /&gt;mingw32-make: *** [sin20200.elf] Error -1073741811&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 10:02:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-1073741811/m-p/1059114#M8302</guid>
      <dc:creator>tony3</dc:creator>
      <dc:date>2020-06-04T10:02:00Z</dc:date>
    </item>
    <item>
      <title>Re: Error -1073741811</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-1073741811/m-p/1059115#M8303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Tony,&lt;/P&gt;&lt;P&gt;I have just created a new project based on MC56F8013, I have tried to compile it, it is okay.&lt;/P&gt;&lt;P&gt;This is the compiling/linking inf on the Console menu of CW tools:&lt;/P&gt;&lt;P&gt;If you new a project based on MC56F8013, then compile/link it on IDE of CW tools, what is the result?&lt;/P&gt;&lt;P&gt;BTW, did you compile an old project or new project?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;**** Clean-only build of configuration FLASH_SDM for project test_8013 ****&lt;BR /&gt;Build complete for project test_8013&lt;/P&gt;&lt;P&gt;**** Build of configuration FLASH_SDM for project test_8013 ****&lt;/P&gt;&lt;P&gt;"C:\\Freescale\\CW MCU v11.1\\gnu\\bin\\mingw32-make" -j8 all &lt;BR /&gt;'Building file: ../Sources/Events.c'&lt;BR /&gt;'Building file: ../Sources/main.c'&lt;BR /&gt;'Building file: ../Project_Settings/Startup_Code/56F80xx_init.asm'&lt;BR /&gt;'Building file: ../Generated_Code/Cpu.c'&lt;BR /&gt;'Building file: ../Generated_Code/Vectors.c'&lt;BR /&gt;'Executing target #1 ../Sources/Events.c'&lt;BR /&gt;'Executing target #2 ../Sources/main.c'&lt;BR /&gt;'Executing target #3 ../Project_Settings/Startup_Code/56F80xx_init.asm'&lt;BR /&gt;'Executing target #4 ../Generated_Code/Cpu.c'&lt;BR /&gt;'Executing target #5 ../Generated_Code/Vectors.c'&lt;BR /&gt;'Invoking: DSC Compiler'&lt;BR /&gt;'Invoking: DSC Compiler'&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e" -c @@"Sources/Events.args" -o "Sources/Events_c.obj" "../Sources/Events.c" -MD -gccdep&lt;BR /&gt;'Invoking: DSC Assembler'&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e" -c @@"Sources/main.args" -o "Sources/main_c.obj" "../Sources/main.c" -MD -gccdep&lt;BR /&gt;'Invoking: DSC Compiler'&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwasm56800e" @@"Project_Settings/Startup_Code/56F80xx_init.args" -o "Project_Settings/Startup_Code/56F80xx_init_asm.obj" "../Project_Settings/Startup_Code/56F80xx_init.asm" -MD -gccdep&lt;BR /&gt;'Invoking: DSC Compiler'&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e" -c @@"Generated_Code/Cpu.args" -o "Generated_Code/Cpu_c.obj" "../Generated_Code/Cpu.c" -MD -gccdep&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e" -c @@"Generated_Code/Vectors.args" -o "Generated_Code/Vectors_c.obj" "../Generated_Code/Vectors.c" -MD -gccdep&lt;BR /&gt;'Finished building: ../Project_Settings/Startup_Code/56F80xx_init.asm'&lt;BR /&gt;' '&lt;BR /&gt;'Finished building: ../Sources/Events.c'&lt;BR /&gt;'Finished building: ../Sources/main.c'&lt;BR /&gt;'Finished building: ../Generated_Code/Cpu.c'&lt;BR /&gt;'Finished building: ../Generated_Code/Vectors.c'&lt;BR /&gt;' '&lt;BR /&gt;' '&lt;BR /&gt;' '&lt;BR /&gt;' '&lt;BR /&gt;'Building target: test_8013.elf'&lt;BR /&gt;'Executing target #6 test_8013.elf'&lt;BR /&gt;'Invoking: DSC Linker'&lt;BR /&gt;"C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwld56800e" -o "test_8013.elf" @@"test_8013.args"&amp;nbsp; &lt;BR /&gt;C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwld56800e|Linker|Warning&lt;BR /&gt;&amp;gt;Overlap of the .interrupt_vectorsboot section and .interrupt_vectors section.&lt;BR /&gt;C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwld56800e|Linker|Warning&lt;BR /&gt;&amp;gt;Overlap of the .interrupt_vectors section and .interrupt_vectorsboot section.&lt;BR /&gt;C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwld56800e|Linker|Warning&lt;BR /&gt;&amp;gt;Binary flash image: P address overlaps with something at word address 0x0&lt;BR /&gt;'Finished building target: test_8013.elf'&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2020 02:24:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-1073741811/m-p/1059115#M8303</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-06-09T02:24:00Z</dc:date>
    </item>
  </channel>
</rss>