<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Tools中的主题 Re: Error:  Couldn't write flash driver to target.  Please make sure that the chip selects are properly configured</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-Couldn-t-write-flash-driver-to-target-Please-make-sure/m-p/1046351#M8253</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A correction: I was trying all of these (the problem i mentioned first) with RCW override method. I made my own override file with my custom board spesific values. I had HRESET OCCURED DURING TRANSACTION error when I used hardcoded-rcw option.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 May 2020 13:23:28 GMT</pubDate>
    <dc:creator>yusufalti333</dc:creator>
    <dc:date>2020-05-22T13:23:28Z</dc:date>
    <item>
      <title>Error:  Couldn't write flash driver to target.  Please make sure that the chip selects are properly configured</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-Couldn-t-write-flash-driver-to-target-Please-make-sure/m-p/1046348#M8250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With using latest Code Warrior, I am trying to flash a new RCW and U-boot into T1042 based new custom board. When I set chipselects to bring up board with hardcoded-rcw, and when I try to flash .bin files to NOR flash, I got this error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Console log&amp;nbsp;from Code Warrior:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fl::target -lc "uboot-core00_SRAM_T1042_Download"&lt;BR /&gt;fl::target -b 0x0 0x40000&lt;BR /&gt;fl::target -v on -l off&lt;BR /&gt;cmdwin::fl::device -d "JS28F00AM29EWL" -o "64Mx16x1" -a 0xe8000000 0xefffffff&lt;BR /&gt;cmdwin::fl::image -f "C:\\Users\\yusuf\\Desktop\\tftpboot\\u-boot-nor-2018.09+fslgit-r0.bin" -t "Binary/Raw Format" -re off -oe on -o 0xeff40000&lt;BR /&gt;cmdwin::fl::erase image&lt;BR /&gt; Beginning Operation ... &lt;BR /&gt;------------------------- &lt;BR /&gt;Performing target initialization ... &lt;BR /&gt;Error: Connect Failed.&lt;BR /&gt;CCS: Connection refused&lt;BR /&gt;[CCS last error: Connection refused ](CCSProtocolPlugin)&lt;BR /&gt;Error: Connect Failed.&lt;BR /&gt;fl::target -lc "uboot-core00_SRAM_T1042_Download"&lt;BR /&gt;fl::target -b 0x0 0x40000&lt;BR /&gt;fl::target -v on -l off&lt;BR /&gt;cmdwin::fl::device -d "JS28F00AM29EWL" -o "64Mx16x1" -a 0xe8000000 0xefffffff&lt;BR /&gt;cmdwin::fl::image -f "C:\\Users\\yusuf\\Desktop\\tftpboot\\u-boot-nor-2018.09+fslgit-r0.bin" -t "Binary/Raw Format" -re off -oe on -o 0xeff40000&lt;BR /&gt;cmdwin::fl::erase image&lt;BR /&gt; Beginning Operation ... &lt;BR /&gt;------------------------- &lt;BR /&gt;Performing target initialization ... &lt;BR /&gt; fe0e0004 &amp;lt;m&amp;gt;0xde000000&amp;lt;/m&amp;gt; .... &lt;BR /&gt; Downloading Flash Device Driver ... &lt;BR /&gt;Error: Couldn't write flash driver to target. Can not read target memory at location: 0x0000000000000000.Please make sure that the chip selects are properly configured. &lt;BR /&gt;The CWPP response code is: CCSProtocolPlugin : Error writing memory &lt;BR /&gt;[CCS last error: Scan timeout ].&lt;BR /&gt;Error: Couldn't write flash driver to target.Can not read target memory at location: 0x0000000000000000.&lt;BR /&gt;Please make sure that the chip selects are properly configured.&lt;BR /&gt;The CWPP response code is: CCSProtocolPlugin : Error writing memory&lt;BR /&gt;[CCS last error: Scan timeout ].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help about this situation ? What could be the reason. I can successfully flash with hardcoded rcw on t1042 demo board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 05:54:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-Couldn-t-write-flash-driver-to-target-Please-make-sure/m-p/1046348#M8250</guid>
      <dc:creator>yusufalti333</dc:creator>
      <dc:date>2020-05-20T05:54:23Z</dc:date>
    </item>
    <item>
      <title>Re: Error:  Couldn't write flash driver to target.  Please make sure that the chip selects are properly configured</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-Couldn-t-write-flash-driver-to-target-Please-make-sure/m-p/1046349#M8251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="345379" data-username="yusufalti333@gmail.com" href="https://community.nxp.com/people/yusufalti333@gmail.com" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 600; text-decoration: none; font-size: 11.9994px;"&gt;Yusuf Altıparmak&lt;/A&gt;&lt;SPAN style="background-color: #ffffff; color: #646464; "&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #646464; "&gt;Please create a bareboard project, in "Debug Target Settings" panel, please select "Download SRAM" Launch configuration.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #646464; "&gt;Then click "RAM" at the right of the project name to select "SRAM", compile the SRAM bareboard project and try whether the executable file&amp;nbsp; can be downloaded&amp;nbsp; and executed in SRAM on the target board successfully.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #646464; "&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #646464; "&gt;Yiping&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 May 2020 08:44:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-Couldn-t-write-flash-driver-to-target-Please-make-sure/m-p/1046349#M8251</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-05-21T08:44:57Z</dc:date>
    </item>
    <item>
      <title>Re: Error:  Couldn't write flash driver to target.  Please make sure that the chip selects are properly configured</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-Couldn-t-write-flash-driver-to-target-Please-make-sure/m-p/1046350#M8252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mr. Wang,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried SRAM option with RCW Override method for my custom board. I am having Scan Timeout when I try to run project like you said. I attached full console log. Do you have any idea about this error ? Could this be about tcl script,It has 2 GB memory map for DDR but I have 16 GB Physical RAM amonunt, should I change it? I am using my DDRCLOCK as 100 MHZ.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is also a Core is not responding error at first lines of log but program seems kept running. Why ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2020 10:45:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-Couldn-t-write-flash-driver-to-target-Please-make-sure/m-p/1046350#M8252</guid>
      <dc:creator>yusufalti333</dc:creator>
      <dc:date>2020-05-22T10:45:36Z</dc:date>
    </item>
    <item>
      <title>Re: Error:  Couldn't write flash driver to target.  Please make sure that the chip selects are properly configured</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-Couldn-t-write-flash-driver-to-target-Please-make-sure/m-p/1046351#M8253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A correction: I was trying all of these (the problem i mentioned first) with RCW override method. I made my own override file with my custom board spesific values. I had HRESET OCCURED DURING TRANSACTION error when I used hardcoded-rcw option.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2020 13:23:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-Couldn-t-write-flash-driver-to-target-Please-make-sure/m-p/1046351#M8253</guid>
      <dc:creator>yusufalti333</dc:creator>
      <dc:date>2020-05-22T13:23:28Z</dc:date>
    </item>
    <item>
      <title>Re: Error:  Couldn't write flash driver to target.  Please make sure that the chip selects are properly configured</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-Couldn-t-write-flash-driver-to-target-Please-make-sure/m-p/1046352#M8254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In your CCS log, you are using&amp;nbsp;T1042RDB_init_core.tcl and there is DDR controller configuration problem on your custom board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I mentioned previously, when&amp;nbsp;&lt;SPAN style="color: #646464; background-color: #ffffff;"&gt;creating a bareboard project, in "Debug Target Settings" panel, please select "Download SRAM" Launch configuration.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #ffffff;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #ffffff;"&gt;Yiping&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 May 2020 09:12:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-Couldn-t-write-flash-driver-to-target-Please-make-sure/m-p/1046352#M8254</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-05-25T09:12:40Z</dc:date>
    </item>
    <item>
      <title>Re: Error:  Couldn't write flash driver to target.  Please make sure that the chip selects are properly configured</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-Couldn-t-write-flash-driver-to-target-Please-make-sure/m-p/1046353#M8255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes,&amp;nbsp; changing .tcl file to init_sram is fixed the problem. For now, I am able to write something to flash.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 10:30:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Error-Couldn-t-write-flash-driver-to-target-Please-make-sure/m-p/1046353#M8255</guid>
      <dc:creator>yusufalti333</dc:creator>
      <dc:date>2020-05-27T10:30:06Z</dc:date>
    </item>
  </channel>
</rss>