<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Unable to debug using JTAG along with multilink in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Unable-to-debug-using-JTAG-along-with-multilink/m-p/1036348#M8223</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, CodeWarrior and PE can be used for this device.&lt;/P&gt;&lt;P&gt;To double check the MCU is not censored, you can try to configure serial boot mode or external boot mode:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103231i1D08D71DB6EA3D45/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;If the device is censored and internal boot mode is selected, the nexus is disabled.&lt;/P&gt;&lt;P&gt;In other modes, there are states when nexus is enabled but flash won't be accessible. You can still see RAM and peripherals. This state can be used for testing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Mar 2020 09:27:06 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2020-03-23T09:27:06Z</dc:date>
    <item>
      <title>Unable to debug using JTAG along with multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Unable-to-debug-using-JTAG-along-with-multilink/m-p/1036347#M8222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using&amp;nbsp;MPC567XEVBMB + MPC5674ADAT516 + SPC5674FMVY3+ PE micro multilink universal + cw 5.9.0 Eval version. Unable to debug. Getting&amp;nbsp;'Cannot Enter Background Mode" error message.&lt;/P&gt;&lt;P&gt;However, Trace32 provides more details.&lt;/P&gt;&lt;P&gt;debug port fail&lt;BR /&gt;JTAGID=0x1827401D&lt;BR /&gt;SYStem.Up error: received invalid OSR (0x000)&lt;BR /&gt; - does the target assert JCOMP while RESET is asserted?&lt;BR /&gt; - is the device censored?&lt;BR /&gt;error: received invalid OSR while core running (0x000)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Whether Codewarrior and PE multilink are good for powerPC???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Mar 2020 20:18:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Unable-to-debug-using-JTAG-along-with-multilink/m-p/1036347#M8222</guid>
      <dc:creator>maddyv</dc:creator>
      <dc:date>2020-03-16T20:18:28Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to debug using JTAG along with multilink</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Unable-to-debug-using-JTAG-along-with-multilink/m-p/1036348#M8223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, CodeWarrior and PE can be used for this device.&lt;/P&gt;&lt;P&gt;To double check the MCU is not censored, you can try to configure serial boot mode or external boot mode:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103231i1D08D71DB6EA3D45/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;If the device is censored and internal boot mode is selected, the nexus is disabled.&lt;/P&gt;&lt;P&gt;In other modes, there are states when nexus is enabled but flash won't be accessible. You can still see RAM and peripherals. This state can be used for testing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2020 09:27:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Unable-to-debug-using-JTAG-along-with-multilink/m-p/1036348#M8223</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2020-03-23T09:27:06Z</dc:date>
    </item>
  </channel>
</rss>