<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Toolsのトピック[CCS last error: T1040: Core not responding ](CCSProtocolPlugin) error after flashing wrong RCW/wrong Place. T1042D4RDB-64B.</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCS-last-error-T1040-Core-not-responding-CCSProtocolPlugin-error/m-p/1031174#M8201</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With using QCSV and T1042D4RDB - 64B,&lt;/P&gt;&lt;P&gt;I accidentally flashed a new RCW into wrong(I guess) place in NOR flash (in both BANK 0 and BANK 4). Now the board is not booting and ASLEEP ping is always lit. When I try to flash a correct RCW (from SDK v2.0 - 1703, rcw_source1400mhz.bin)&amp;nbsp; into correct place, CW is throwing;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;[CCS last error: T1040: Core not responding ](CCSProtocolPlugin) error&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Switch settings were,&lt;/P&gt;&lt;P&gt;SW1: 0001 0011&lt;/P&gt;&lt;P&gt;SW2: 1011 1001&lt;/P&gt;&lt;P&gt;SW3: 1110 0001&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After crahsing first bank, I changed SW[3] to 1 to jump on BANK4. I did same mistake on BANK4. I was trying to write offset 0xE801FFFF which is the end adress of RCW (current bank), not start adress. Now I am not able to use both BANK0 and BANK4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using latest Code Warrior.&lt;/P&gt;&lt;P&gt;I will be appriciated for any help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Feb 2020 11:29:43 GMT</pubDate>
    <dc:creator>yusufalti4444</dc:creator>
    <dc:date>2020-02-03T11:29:43Z</dc:date>
    <item>
      <title>[CCS last error: T1040: Core not responding ](CCSProtocolPlugin) error after flashing wrong RCW/wrong Place. T1042D4RDB-64B.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCS-last-error-T1040-Core-not-responding-CCSProtocolPlugin-error/m-p/1031174#M8201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With using QCSV and T1042D4RDB - 64B,&lt;/P&gt;&lt;P&gt;I accidentally flashed a new RCW into wrong(I guess) place in NOR flash (in both BANK 0 and BANK 4). Now the board is not booting and ASLEEP ping is always lit. When I try to flash a correct RCW (from SDK v2.0 - 1703, rcw_source1400mhz.bin)&amp;nbsp; into correct place, CW is throwing;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;[CCS last error: T1040: Core not responding ](CCSProtocolPlugin) error&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Switch settings were,&lt;/P&gt;&lt;P&gt;SW1: 0001 0011&lt;/P&gt;&lt;P&gt;SW2: 1011 1001&lt;/P&gt;&lt;P&gt;SW3: 1110 0001&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After crahsing first bank, I changed SW[3] to 1 to jump on BANK4. I did same mistake on BANK4. I was trying to write offset 0xE801FFFF which is the end adress of RCW (current bank), not start adress. Now I am not able to use both BANK0 and BANK4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using latest Code Warrior.&lt;/P&gt;&lt;P&gt;I will be appriciated for any help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Feb 2020 11:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCS-last-error-T1040-Core-not-responding-CCSProtocolPlugin-error/m-p/1031174#M8201</guid>
      <dc:creator>yusufalti4444</dc:creator>
      <dc:date>2020-02-03T11:29:43Z</dc:date>
    </item>
    <item>
      <title>Re: [CCS last error: T1040: Core not responding ](CCSProtocolPlugin) error after flashing wrong RCW/wrong Place. T1042D4RDB-64B.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCS-last-error-T1040-Core-not-responding-CCSProtocolPlugin-error/m-p/1031175#M8202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/yipingwang"&gt;yipingwang&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;Update: It seems I loaded a working RCW on NOR flash BANK0 with using Hardcoded-RCW option (SW1 - SW2[0] = 010011011 where 0 = ON). Asleep led is not lighting when I select BANK0. I flashed RCW to 0xE8000000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But now,&amp;nbsp; I can not do same flashing to BANK4 (0xEC000000 is RCW adress of BANK4). When I switch back to BANK4 after flashing working RCW to BANK4, asleep led is lighting. CodeWarrior seems not flashing to BANK4 memory area.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I flashed a working U-boot to BANK0 U-boot area (0xEFF40000 for BANK0). I do not get any serial output from U-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is wrong with my Flash programmer ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Feb 2020 06:25:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCS-last-error-T1040-Core-not-responding-CCSProtocolPlugin-error/m-p/1031175#M8202</guid>
      <dc:creator>yusufalti4444</dc:creator>
      <dc:date>2020-02-04T06:25:59Z</dc:date>
    </item>
    <item>
      <title>Re: [CCS last error: T1040: Core not responding ](CCSProtocolPlugin) error after flashing wrong RCW/wrong Place. T1042D4RDB-64B.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCS-last-error-T1040-Core-not-responding-CCSProtocolPlugin-error/m-p/1031176#M8203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="352589" data-username="yusufalti4444@gmail.com" href="https://community.nxp.com/people/yusufalti4444@gmail.com"&gt;Ahmet Demir&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First please create a bareboard project in CodeWarrior IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to the section "8.4 Setting up a remote system to use a JTAG configuration file" in Freescale\CW_PA_v10.5.1\PA\Help\PDF\Targeting_PA_Processors.pdf to use CodeWarrior JTAG configuration file to override RCW on the target board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After configuring JTAG Configuration file in CodeWarrior IDE, please open "Hardware or Simulator Connection" panel from Run-&amp;gt;Debug Configuration-&amp;gt;&amp;lt;project&amp;gt;-core00_RAM_T1042_Connect/Download-&amp;gt;Edit-&amp;gt;Edit, please check "Initialize target" and specify "Initialize target script" as ${ProjDirPath}/CFG/T1042RDB_init_core.tcl.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then connect CodeWarrior to the target board to do flash programming.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Feb 2020 07:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCS-last-error-T1040-Core-not-responding-CCSProtocolPlugin-error/m-p/1031176#M8203</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-02-04T07:40:23Z</dc:date>
    </item>
  </channel>
</rss>