<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: Using NTAG I2C chip with frdm-kl03z</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001425#M8047</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't think the Ram settings changed automatically when I changed the MCU from the KL02z to the KL03Z&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Dec 2019 18:55:36 GMT</pubDate>
    <dc:creator>darren</dc:creator>
    <dc:date>2019-12-05T18:55:36Z</dc:date>
    <item>
      <title>Using NTAG I2C chip with frdm-kl03z</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001419#M8041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with the NTAG&amp;nbsp;&lt;SPAN style="font-size: 12.5pt; color: #1a1a1a;"&gt;NT3H2111W0FHKH I am trying to get it to work with the frdm-kl03z development board but I am having issues with the code throwing hard faults. I have adjusted the example code that comes with the NTAG explorer board and works with LPC line of microprocessors. The code runs but will throw faults when writing to a memory address. I believe this may be an issue with the I2C base address. What should I set the base address in order to avoid throwing hard faults? Any help would be great.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Dec 2019 20:59:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001419#M8041</guid>
      <dc:creator>darren</dc:creator>
      <dc:date>2019-12-03T20:59:49Z</dc:date>
    </item>
    <item>
      <title>Re: Using NTAG I2C chip with frdm-kl03z</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001420#M8042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can try using the KL02 example as a base, when you are building the SDK for the FRDM-KL03 you can see this :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92735iF93E9C56F5D69B25/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;You can try to copy the folders in your project and add the different initialization, could you please check it and try this approach&amp;nbsp; and try to run the example&amp;nbsp; there in your device ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;BR /&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2019 17:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001420#M8042</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-12-04T17:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: Using NTAG I2C chip with frdm-kl03z</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001421#M8043</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;BR /&gt;Thanks for the reply. Super helpful.&lt;BR /&gt;I did this and got the code to compile, but when I go to debug it throws a hard fault before reaching the main function.&amp;nbsp;&lt;BR /&gt;The fault says,&amp;nbsp;&lt;/P&gt;&lt;P&gt;"Break at address "0x1c001ed4" with no debug information available, or outside of program code"&lt;/P&gt;&lt;P&gt;it there any experience with this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2019 20:31:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001421#M8043</guid>
      <dc:creator>darren</dc:creator>
      <dc:date>2019-12-04T20:31:09Z</dc:date>
    </item>
    <item>
      <title>Re: Using NTAG I2C chip with frdm-kl03z</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001422#M8044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does it happen with the demo or driver examples as well ? Or is it only with your code migration/NTAG implementation ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards ,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2019 21:47:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001422#M8044</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-12-04T21:47:22Z</dc:date>
    </item>
    <item>
      <title>Re: Using NTAG I2C chip with frdm-kl03z</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001423#M8045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #222222; background-color: #ffffff; font-size: small;"&gt;I got the hard fault fixed by changing the RAM location in the MCU settings. However, the code keeps getting hung up&amp;nbsp;on the setup function when trying to execute the line&amp;nbsp;&amp;nbsp;HAL_ISR_&lt;/SPAN&gt;&lt;SPAN style="color: #222222; background-color: #ffffff; font-size: small;"&gt;RegisterCallback((ISR_SOURCE_&lt;/SPAN&gt;&lt;SPAN style="color: #222222; background-color: #ffffff; font-size: small;"&gt;T)0, ISR_LEVEL_LO, NULL, NULL);. When I step into the function the code seems to hang up&amp;nbsp;on the line&amp;nbsp;enableInterrupt(callback-&lt;/SPAN&gt;&lt;SPAN style="color: #222222; background-color: #ffffff; font-size: small;"&gt;&amp;gt;channel);&amp;nbsp;&lt;/SPAN&gt;&lt;BR style="color: #222222; background-color: #ffffff; font-size: small;" /&gt;&lt;SPAN style="color: #222222; background-color: #ffffff; font-size: small;"&gt;I am not sure why this is happening&amp;nbsp;or how to rectify this.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Dec 2019 15:40:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001423#M8045</guid>
      <dc:creator>darren</dc:creator>
      <dc:date>2019-12-05T15:40:03Z</dc:date>
    </item>
    <item>
      <title>Re: Using NTAG I2C chip with frdm-kl03z</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001424#M8046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't understand why you had to change the RAM configuration if you use the KL03Z as a base all the configurations and functions of the i2c polling example (if you imported that) should be already there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you did not use the i2c polling as a base, which one you used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Dec 2019 18:53:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001424#M8046</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-12-05T18:53:20Z</dc:date>
    </item>
    <item>
      <title>Re: Using NTAG I2C chip with frdm-kl03z</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001425#M8047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't think the Ram settings changed automatically when I changed the MCU from the KL02z to the KL03Z&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Dec 2019 18:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001425#M8047</guid>
      <dc:creator>darren</dc:creator>
      <dc:date>2019-12-05T18:55:36Z</dc:date>
    </item>
    <item>
      <title>Re: Using NTAG I2C chip with frdm-kl03z</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001426#M8048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure if you modified all the necessary elements and if all the necessary elements in the project configurations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend you to use one of the I2C examples in the SDK, copy the HAL folders as well as the NTAG I2C folder and the source folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this way, you already have all the project configured correctly, and you will only need to add the folders to the project path&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/95699iC086E22F31AFE0EC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_9.png" alt="pastedImage_9.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards ,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Dec 2019 20:33:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001426#M8048</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-12-05T20:33:06Z</dc:date>
    </item>
    <item>
      <title>Re: Using NTAG I2C chip with frdm-kl03z</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001427#M8049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I ended up having to change the startup files and the preprocessor steps. It is working now thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Dec 2019 22:50:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Using-NTAG-I2C-chip-with-frdm-kl03z/m-p/1001427#M8049</guid>
      <dc:creator>darren</dc:creator>
      <dc:date>2019-12-06T22:50:32Z</dc:date>
    </item>
  </channel>
</rss>