<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Tools中的主题 USB TAP ONCE breakpoint</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/USB-TAP-ONCE-breakpoint/m-p/235275#M78</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;Anyone know why using the USB TAP ONCE unit and setting BP instead of showing me the code at the BP marker the debugger jump to internal interrupt?&lt;/P&gt;&lt;P&gt;Picture attached.&lt;/P&gt;&lt;P&gt;I tried using PEmicro Multilink Universal instead and it run OK.&lt;/P&gt;&lt;P&gt;I had the same problem with 2 USB TAO units I tested (revB)&lt;/P&gt;&lt;P&gt;I even tried to reset the USB TAP unit according to the manual instructions, but it did not help.&lt;/P&gt;&lt;P&gt;TIA&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Feb 2014 09:24:58 GMT</pubDate>
    <dc:creator>Ben</dc:creator>
    <dc:date>2014-02-14T09:24:58Z</dc:date>
    <item>
      <title>USB TAP ONCE breakpoint</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/USB-TAP-ONCE-breakpoint/m-p/235275#M78</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;Anyone know why using the USB TAP ONCE unit and setting BP instead of showing me the code at the BP marker the debugger jump to internal interrupt?&lt;/P&gt;&lt;P&gt;Picture attached.&lt;/P&gt;&lt;P&gt;I tried using PEmicro Multilink Universal instead and it run OK.&lt;/P&gt;&lt;P&gt;I had the same problem with 2 USB TAO units I tested (revB)&lt;/P&gt;&lt;P&gt;I even tried to reset the USB TAP unit according to the manual instructions, but it did not help.&lt;/P&gt;&lt;P&gt;TIA&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2014 09:24:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/USB-TAP-ONCE-breakpoint/m-p/235275#M78</guid>
      <dc:creator>Ben</dc:creator>
      <dc:date>2014-02-14T09:24:58Z</dc:date>
    </item>
    <item>
      <title>Re: USB TAP ONCE breakpoint</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/USB-TAP-ONCE-breakpoint/m-p/235276#M79</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000;"&gt;Please delete .metadata folder of workspace of CW 10.5.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000;"&gt;Then reopen the project in CodeWarrior, and click on 'Project' menu-&amp;gt; Clean to remove the old object file, and then rebuild the project. Is the problem fixed? &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2014 11:01:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/USB-TAP-ONCE-breakpoint/m-p/235276#M79</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2014-02-17T11:01:19Z</dc:date>
    </item>
    <item>
      <title>Re: USB TAP ONCE breakpoint</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/USB-TAP-ONCE-breakpoint/m-p/235277#M80</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Fiona,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you found out, there is a bug with the USB TAP ONCE that cause it.&lt;/P&gt;&lt;P&gt;Thank you for confirming it on the S/R, it's a pity that you don't publish this fact here to prevent community users to waist time on such bug.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2014 23:48:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/USB-TAP-ONCE-breakpoint/m-p/235277#M80</guid>
      <dc:creator>Ben</dc:creator>
      <dc:date>2014-02-19T23:48:02Z</dc:date>
    </item>
  </channel>
</rss>