<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Type of output file is necessary to load to the program in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Type-of-output-file-is-necessary-to-load-to-the-program/m-p/939024#M7794</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using CodeWarrior v8.3 for programming of DSP56807 controller with Codewarrior USB TAP ONCE debugger, I am unable to understand what type of output file is necessary to load to the program.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Oct 2019 06:21:14 GMT</pubDate>
    <dc:creator>sujaigowda</dc:creator>
    <dc:date>2019-10-03T06:21:14Z</dc:date>
    <item>
      <title>Type of output file is necessary to load to the program</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Type-of-output-file-is-necessary-to-load-to-the-program/m-p/939024#M7794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using CodeWarrior v8.3 for programming of DSP56807 controller with Codewarrior USB TAP ONCE debugger, I am unable to understand what type of output file is necessary to load to the program.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 06:21:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Type-of-output-file-is-necessary-to-load-to-the-program/m-p/939024#M7794</guid>
      <dc:creator>sujaigowda</dc:creator>
      <dc:date>2019-10-03T06:21:14Z</dc:date>
    </item>
    <item>
      <title>Re: Type of output file is necessary to load to the program</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Type-of-output-file-is-necessary-to-load-to-the-program/m-p/939025#M7795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Sujai,&lt;/P&gt;&lt;P&gt;The CW tools can generate the *.elf file, which you can click "debug" in CW for DSP56800E tools&amp;nbsp; to download&amp;nbsp; to flash of DSP56F807.&lt;/P&gt;&lt;P&gt;As the following Fig, the first file Flash is elf file, the extension name is "elf".&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/57029iF6FFE5F4EF8BE2EE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 08:41:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Type-of-output-file-is-necessary-to-load-to-the-program/m-p/939025#M7795</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-10-08T08:41:03Z</dc:date>
    </item>
  </channel>
</rss>