<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Tools中的主题 Re: FRDM-KE06Z with Codewarrior 10.6</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FRDM-KE06Z-with-Codewarrior-10-6/m-p/307739#M771</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah, I think that was the key.&amp;nbsp; I didn't realize that default option for the console I/O was the problem.&amp;nbsp; Thanks! &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 May 2014 12:23:40 GMT</pubDate>
    <dc:creator>davidsherman</dc:creator>
    <dc:date>2014-05-06T12:23:40Z</dc:date>
    <item>
      <title>FRDM-KE06Z with Codewarrior 10.6</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FRDM-KE06Z-with-Codewarrior-10-6/m-p/307734#M766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #333333;"&gt;I have the FRDM-KE06Z, and I have succeeded in getting the debugger working through OpenSDA.&amp;nbsp; I was able to run a simple application and toggle the LED.&amp;nbsp; When I generate an S-record output and give it a .srec extension, I have tried programming it through the MSD programmer and through CodeWarrior, but no LED.&amp;nbsp; I also tried programming the lab_demo_frdm.srec from the KE06Z Quick Start Package, but it doesn't seem to do anything.&amp;nbsp; I have the&lt;/SPAN&gt;&lt;SPAN style="color: #333333; font-size: 10pt;"&gt; &lt;SPAN style="color: #333333;"&gt;PEMicro FRDM-KE06Z Mass Storage/Debug App Version 1.14 installed.&amp;nbsp; Is the lab_demo_frdm.srec the same demo which came loaded on the board?&amp;nbsp; Thanks!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Apr 2014 19:16:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FRDM-KE06Z-with-Codewarrior-10-6/m-p/307734#M766</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2014-04-30T19:16:34Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KE06Z with Codewarrior 10.6</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FRDM-KE06Z-with-Codewarrior-10-6/m-p/307735#M767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The lab_demo_frmd.srec is the same example which is loaded by default in your FRDM platform. If you have the Storage/Debug sda application then your device must appear as a MSD device in the windows explorer. If you want to download an s19/srec file you have to generate it in CodeWarrior (&lt;A href="http://mcuoneclipse.com/2012/09/13/s-record-generation-with-gcc-for-armkinetis/" title="http://mcuoneclipse.com/2012/09/13/s-record-generation-with-gcc-for-armkinetis/"&gt;S-Record Generation with gcc for ARM/Kinetis | MCU on Eclipse&lt;/A&gt;), this s19 file has an extension .hex. If you want to download this in your device drag and drop it (.hex file) into the device (the MSD one).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can try also to download again the .sda application. Enter your device in Bootloader mode and drag and drop the .sda application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information can help you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. It would be nice!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Apr 2014 22:28:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FRDM-KE06Z-with-Codewarrior-10-6/m-p/307735#M767</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2014-04-30T22:28:08Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KE06Z with Codewarrior 10.6</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FRDM-KE06Z-with-Codewarrior-10-6/m-p/307736#M768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Adrian, I have tried updating the OpenSDA application again, and reconnected the USB cable. When I drag and drop the lab_demo_frdm.srec into the FRDM_KE06Z folder, it appears to copy, but nothing happens after that.&amp;nbsp; I can still run my application through the debugger.&amp;nbsp; Is there a way to verify the flash contents to see if it programmed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edit:&amp;nbsp; I was able to use the flash programmer from within CodeWarrior to reprogram the lab_dem_frdm.srec, and that is working again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 May 2014 12:43:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FRDM-KE06Z-with-Codewarrior-10-6/m-p/307736#M768</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2014-05-01T12:43:19Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KE06Z with Codewarrior 10.6</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FRDM-KE06Z-with-Codewarrior-10-6/m-p/307737#M769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've narrowed it down, and I can use the MSD to write to the flash.&amp;nbsp; I can install the lab_demo_frdm.srec, and I was able to build the platinum project example to get the LED to blink.&amp;nbsp; A problem I'm still running into is if I create a new project from scratch, I can only run it over the debugger.&amp;nbsp; I can change the PC to __thumb_startup, and it will run successfully into main().&amp;nbsp; If I let it run out of flash, it seems to have problems when it reaches __init_semihost.&amp;nbsp; If I turn on the LED just before the call to that, it works.&amp;nbsp; If I try to turn on the LED after the call, it does not turn on.&amp;nbsp; Am I missing something?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 May 2014 20:44:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FRDM-KE06Z-with-Codewarrior-10-6/m-p/307737#M769</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2014-05-01T20:44:45Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KE06Z with Codewarrior 10.6</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FRDM-KE06Z-with-Codewarrior-10-6/m-p/307738#M770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess the problem is with the libraries. You are using one of the hosted options. Check the next thread for the same problem:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/391778"&gt;Re: MK10DX256VLK7 doesn't run standalone, just when debugging. Verified it's running from FLASH, not RAM.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to select one for the libraries that do not end with "..hosted"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 May 2014 23:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FRDM-KE06Z-with-Codewarrior-10-6/m-p/307738#M770</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-05-04T23:34:33Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KE06Z with Codewarrior 10.6</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FRDM-KE06Z-with-Codewarrior-10-6/m-p/307739#M771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah, I think that was the key.&amp;nbsp; I didn't realize that default option for the console I/O was the problem.&amp;nbsp; Thanks! &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 May 2014 12:23:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/FRDM-KE06Z-with-Codewarrior-10-6/m-p/307739#M771</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2014-05-06T12:23:40Z</dc:date>
    </item>
  </channel>
</rss>