<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Tools中的主题 Re: code warrior runtime project files</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-warrior-runtime-project-files/m-p/307454#M765</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Main Standard Libraries (MSL) are complete, configurable set of C and C++ standard libraries. So this library is necessary if using C or C++ to develop project. &lt;/P&gt;&lt;P&gt;To use the MSL library, you must also use a runtime library. A runtime library provides low-level functions that support high-level C and C++ language features, such as memory management and file system access.&lt;/P&gt;&lt;P&gt;For details, please refer to &amp;lt;Chapter 23 Libraries and Support Code&amp;gt; in Power Architecture Build Tools Reference, usually is:&lt;/P&gt;&lt;P&gt;C:\Program Files\Freescale\CW for MPC55xx and MPC56xx 2.10\Help\PDF\Power Architecture Build Tools Reference.pdf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Apr 2014 10:10:57 GMT</pubDate>
    <dc:creator>TICS_Fiona</dc:creator>
    <dc:date>2014-04-03T10:10:57Z</dc:date>
    <item>
      <title>code warrior runtime project files</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-warrior-runtime-project-files/m-p/307453#M764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="10582_10582.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119757iC26BBF733B8419D0/image-size/large?v=v2&amp;amp;px=999" role="button" title="10582_10582.png" alt="10582_10582.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="aaaaa.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43377i1F0DB666B76D2357/image-size/large?v=v2&amp;amp;px=999" role="button" title="aaaaa.png" alt="aaaaa.png" /&gt;&lt;/span&gt;&lt;BR /&gt;When I create a new project with the wizard in Code Warrior, as shown above some runtime library files are added.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What are they? Can I create and build my project without them?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best reagrds&lt;/P&gt;&lt;P&gt;izzet&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2014 06:29:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-warrior-runtime-project-files/m-p/307453#M764</guid>
      <dc:creator>izzetozcelik</dc:creator>
      <dc:date>2014-04-01T06:29:40Z</dc:date>
    </item>
    <item>
      <title>Re: code warrior runtime project files</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-warrior-runtime-project-files/m-p/307454#M765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Main Standard Libraries (MSL) are complete, configurable set of C and C++ standard libraries. So this library is necessary if using C or C++ to develop project. &lt;/P&gt;&lt;P&gt;To use the MSL library, you must also use a runtime library. A runtime library provides low-level functions that support high-level C and C++ language features, such as memory management and file system access.&lt;/P&gt;&lt;P&gt;For details, please refer to &amp;lt;Chapter 23 Libraries and Support Code&amp;gt; in Power Architecture Build Tools Reference, usually is:&lt;/P&gt;&lt;P&gt;C:\Program Files\Freescale\CW for MPC55xx and MPC56xx 2.10\Help\PDF\Power Architecture Build Tools Reference.pdf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Apr 2014 10:10:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/code-warrior-runtime-project-files/m-p/307454#M765</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2014-04-03T10:10:57Z</dc:date>
    </item>
  </channel>
</rss>