<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Tools中的主题 Re: ADC - Problem in sensing voltage</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/ADC-Problem-in-sensing-voltage/m-p/908340#M7634</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Padma,&lt;/P&gt;&lt;P&gt;Anyway, as you know that the ADC analog channel pin is an input pin, I think it does not make sense to test the voltage of ADC analog channel pin when the ADC analog channel pin is float. If you want to convert ADC analog channel, you have to connect a low impedance voltage source to the ADC analog channel pin.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 May 2019 05:55:50 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2019-05-14T05:55:50Z</dc:date>
    <item>
      <title>ADC - Problem in sensing voltage</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/ADC-Problem-in-sensing-voltage/m-p/908338#M7632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In my project I am using all the 16 ADC channels, facing problem in sensing the exact voltage values.&lt;/P&gt;&lt;P&gt;Have checked with voltage variations from 0v - 3.3v , my reference voltage is 3.3v.&lt;/P&gt;&lt;P&gt;My questions is:&lt;/P&gt;&lt;P&gt;while (in&amp;nbsp;ADC Control Register 1 (ADCR1)) using once sequential or once simultaneous mode and triggered sequential and triggered sequential mode I can get the variation from 0v - 3.3v. But while using loop sequential or loop simultaneous mode even if I dint give any voltage input to adc it is automatically producing 1.2v-1.5v. How is this possible? It is not because of the circuit as I have not connected any sensor or input unit to channels.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have gone through datasheet and user guide but I'm not clear. Can any one explain in detail?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 May 2019 13:04:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/ADC-Problem-in-sensing-voltage/m-p/908338#M7632</guid>
      <dc:creator>padmaashok765</dc:creator>
      <dc:date>2019-05-11T13:04:05Z</dc:date>
    </item>
    <item>
      <title>Re: ADC - Problem in sensing voltage</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/ADC-Problem-in-sensing-voltage/m-p/908339#M7633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry I am using MC56F8367 .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 04:34:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/ADC-Problem-in-sensing-voltage/m-p/908339#M7633</guid>
      <dc:creator>padmaashok765</dc:creator>
      <dc:date>2019-05-13T04:34:14Z</dc:date>
    </item>
    <item>
      <title>Re: ADC - Problem in sensing voltage</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/ADC-Problem-in-sensing-voltage/m-p/908340#M7634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Padma,&lt;/P&gt;&lt;P&gt;Anyway, as you know that the ADC analog channel pin is an input pin, I think it does not make sense to test the voltage of ADC analog channel pin when the ADC analog channel pin is float. If you want to convert ADC analog channel, you have to connect a low impedance voltage source to the ADC analog channel pin.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 May 2019 05:55:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/ADC-Problem-in-sensing-voltage/m-p/908340#M7634</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-05-14T05:55:50Z</dc:date>
    </item>
  </channel>
</rss>