<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic codewarrior only call the lib file which generated by itself? in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/codewarrior-only-call-the-lib-file-which-generated-by-itself/m-p/904857#M7615</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recently used the mpu9250 axis attitude sensor, and I used the MC9S12XEP100 chip to develop in the codewarrior 5.9 environment. When I call the lib file provided by the MPU9250, the codewarrior always reports an error: L1934:ELF:Request is not valid&lt;BR /&gt;The lib file is used in the keil environment without problems.&lt;BR /&gt;Can codewarrior only call the lib file generated by itself?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Apr 2019 01:36:57 GMT</pubDate>
    <dc:creator>yongpanan</dc:creator>
    <dc:date>2019-04-23T01:36:57Z</dc:date>
    <item>
      <title>codewarrior only call the lib file which generated by itself?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/codewarrior-only-call-the-lib-file-which-generated-by-itself/m-p/904857#M7615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recently used the mpu9250 axis attitude sensor, and I used the MC9S12XEP100 chip to develop in the codewarrior 5.9 environment. When I call the lib file provided by the MPU9250, the codewarrior always reports an error: L1934:ELF:Request is not valid&lt;BR /&gt;The lib file is used in the keil environment without problems.&lt;BR /&gt;Can codewarrior only call the lib file generated by itself?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Apr 2019 01:36:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/codewarrior-only-call-the-lib-file-which-generated-by-itself/m-p/904857#M7615</guid>
      <dc:creator>yongpanan</dc:creator>
      <dc:date>2019-04-23T01:36:57Z</dc:date>
    </item>
    <item>
      <title>Re: codewarrior only call the lib file which generated by itself?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/codewarrior-only-call-the-lib-file-which-generated-by-itself/m-p/904858#M7616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="306728" data-username="yongpanan" href="https://community.nxp.com/people/yongpanan"&gt;Yongpan An&lt;/A&gt;&lt;/P&gt;&lt;P&gt;You are right.CodeWarrior only calls the lib generated by itself.&lt;/P&gt;&lt;P&gt;For example, your app is developed under CodeWarrior v5.2, the lib should also be built under this version also.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Apr 2019 05:24:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/codewarrior-only-call-the-lib-file-which-generated-by-itself/m-p/904858#M7616</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-04-23T05:24:29Z</dc:date>
    </item>
    <item>
      <title>Re: codewarrior only call the lib file which generated by itself?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/codewarrior-only-call-the-lib-file-which-generated-by-itself/m-p/904859#M7617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="15013" data-username="ZhangJennie" href="https://community.nxp.com/people/ZhangJennie" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: underline; font-size: 1.286rem;"&gt;ZhangJennie&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I got it.Thanks for you help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Apr 2019 00:00:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/codewarrior-only-call-the-lib-file-which-generated-by-itself/m-p/904859#M7617</guid>
      <dc:creator>yongpanan</dc:creator>
      <dc:date>2019-04-26T00:00:56Z</dc:date>
    </item>
    <item>
      <title>Re: codewarrior only call the lib file which generated by itself?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/codewarrior-only-call-the-lib-file-which-generated-by-itself/m-p/904860#M7618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are welcome!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Apr 2019 01:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/codewarrior-only-call-the-lib-file-which-generated-by-itself/m-p/904860#M7618</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-04-26T01:47:28Z</dc:date>
    </item>
  </channel>
</rss>