<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: how to program T4240RDB flash connection based our custom board using codewarrior Flash programmer</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-program-T4240RDB-flash-connection-based-our-custom-board/m-p/860053#M7373</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pavel!&lt;/P&gt;&lt;P&gt;Do you think that amd16x2.elf (64Mx16x2) not suitable to program our flash as connected(as per screenshot). Because almost all operation works fine except write operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you suggested we took&amp;nbsp; AMD16x1Example and just compile it then used the created .elf on&amp;nbsp;T4240RDB. In this process we got following error.&lt;/P&gt;&lt;P&gt;fl::target -lc "AMD16x1Example Flash Algo Development "&lt;BR /&gt;fl::target -b 0x0 0x180000&lt;BR /&gt;fl::target -v off -l off&lt;BR /&gt;cmdwin::fl::device -d "S29GL01GP-cor" -o "64Mx16x1" -a 0xe8000000 0xefffffff&lt;BR /&gt;cmdwin::fl::diagnose&lt;BR /&gt;&amp;nbsp;Beginning Operation ...&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;------------------------- &lt;BR /&gt;Performing target initialization ...&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;Downloading Flash Diagnostics Driver ...&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;Reading flash ID .......&lt;BR /&gt;Error:&amp;nbsp; The algorithm was not able to run on the target or the flash is not configured properly.&lt;BR /&gt;Error:&amp;nbsp; Getting flash ID failed&lt;BR /&gt;Error: The algorithm was not able to run on the target or the flash is not configured properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This should be work first because this is tested on T4240RDB board having&amp;nbsp; only one S29GL01GS(AMD16x1). If it works then we make corresponding changes for our flash configuration or can you give us corresponding algorithm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;K dhanasekaran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Feb 2019 07:04:01 GMT</pubDate>
    <dc:creator>dhanasekaran</dc:creator>
    <dc:date>2019-02-05T07:04:01Z</dc:date>
    <item>
      <title>how to program T4240RDB flash connection based our custom board using codewarrior Flash programmer</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-program-T4240RDB-flash-connection-based-our-custom-board/m-p/860051#M7371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone!&lt;/P&gt;&lt;P&gt;In out custom board we are using two flash chips are connected with T4240 as shown in below attachment. we tried to flash it using amd16x2.elf (64Mx16x2) via flash programmer, It provides sector protect error But Erase , Dump and Diagnose test are performed successfully during write operation it reports error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;used IDE: codewarrior 10.5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Give us your suggestion Thank you,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;K dhanasekaran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2019 15:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-program-T4240RDB-flash-connection-based-our-custom-board/m-p/860051#M7371</guid>
      <dc:creator>dhanasekaran</dc:creator>
      <dc:date>2019-01-24T15:13:26Z</dc:date>
    </item>
    <item>
      <title>Re: how to program T4240RDB flash connection based our custom board using codewarrior Flash programmer</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-program-T4240RDB-flash-connection-based-our-custom-board/m-p/860052#M7372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;Add new device to the CodeWarrior Flash Programmer for your Flash configuration.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;See the "AppNote-FlashProgrammer-PowerArchitecture.pdf" file in CodeWarrior folder:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;C:\Freescale\CW_PA_v10.5.1\PA\PA_Tools\FlashToolKit\Documentation&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2019 06:06:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-program-T4240RDB-flash-connection-based-our-custom-board/m-p/860052#M7372</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2019-02-05T06:06:27Z</dc:date>
    </item>
    <item>
      <title>Re: how to program T4240RDB flash connection based our custom board using codewarrior Flash programmer</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-program-T4240RDB-flash-connection-based-our-custom-board/m-p/860053#M7373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pavel!&lt;/P&gt;&lt;P&gt;Do you think that amd16x2.elf (64Mx16x2) not suitable to program our flash as connected(as per screenshot). Because almost all operation works fine except write operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you suggested we took&amp;nbsp; AMD16x1Example and just compile it then used the created .elf on&amp;nbsp;T4240RDB. In this process we got following error.&lt;/P&gt;&lt;P&gt;fl::target -lc "AMD16x1Example Flash Algo Development "&lt;BR /&gt;fl::target -b 0x0 0x180000&lt;BR /&gt;fl::target -v off -l off&lt;BR /&gt;cmdwin::fl::device -d "S29GL01GP-cor" -o "64Mx16x1" -a 0xe8000000 0xefffffff&lt;BR /&gt;cmdwin::fl::diagnose&lt;BR /&gt;&amp;nbsp;Beginning Operation ...&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;------------------------- &lt;BR /&gt;Performing target initialization ...&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;Downloading Flash Diagnostics Driver ...&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;Reading flash ID .......&lt;BR /&gt;Error:&amp;nbsp; The algorithm was not able to run on the target or the flash is not configured properly.&lt;BR /&gt;Error:&amp;nbsp; Getting flash ID failed&lt;BR /&gt;Error: The algorithm was not able to run on the target or the flash is not configured properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This should be work first because this is tested on T4240RDB board having&amp;nbsp; only one S29GL01GS(AMD16x1). If it works then we make corresponding changes for our flash configuration or can you give us corresponding algorithm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;K dhanasekaran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2019 07:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-program-T4240RDB-flash-connection-based-our-custom-board/m-p/860053#M7373</guid>
      <dc:creator>dhanasekaran</dc:creator>
      <dc:date>2019-02-05T07:04:01Z</dc:date>
    </item>
    <item>
      <title>Re: how to program T4240RDB flash connection based our custom board using codewarrior Flash programmer</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-program-T4240RDB-flash-connection-based-our-custom-board/m-p/860054#M7374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-left: 0.5in; margin-bottom: 0in; line-height: 100%;"&gt;Hi pavel!&lt;/P&gt;&lt;P style="margin-left: 0.5in; margin-bottom: 0in; line-height: 100%;"&gt;&lt;/P&gt;&lt;P style="margin-left: 0.5in; margin-bottom: 0in; line-height: 100%;"&gt;Can u share source of amd16x1.elf and amd16x2.elf files?&lt;/P&gt;&lt;P style="margin-left: 0.5in; margin-bottom: 0in; line-height: 100%;"&gt;&lt;/P&gt;&lt;P style="margin-left: 0.5in; margin-bottom: 0in; line-height: 100%;"&gt;&lt;/P&gt;&lt;P style="margin-left: 0.5in; margin-bottom: 0in; line-height: 100%;"&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;K dhanasekaran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2019 14:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-program-T4240RDB-flash-connection-based-our-custom-board/m-p/860054#M7374</guid>
      <dc:creator>dhanasekaran</dc:creator>
      <dc:date>2019-02-14T14:55:36Z</dc:date>
    </item>
    <item>
      <title>Re: how to program T4240RDB flash connection based our custom board using codewarrior Flash programmer</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-program-T4240RDB-flash-connection-based-our-custom-board/m-p/860055#M7375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;No one else has this question?&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Feb 2019 10:22:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-program-T4240RDB-flash-connection-based-our-custom-board/m-p/860055#M7375</guid>
      <dc:creator>dhanasekaran</dc:creator>
      <dc:date>2019-02-18T10:22:12Z</dc:date>
    </item>
  </channel>
</rss>