<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: MPC8309 Custom board with NandFlash</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MPC8309-Custom-board-with-NandFlash/m-p/808104#M7036</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i am seeing the following error&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Performing target initialization ...&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;Error:&amp;nbsp; Connect Failed.&lt;BR /&gt;Failed to reset the target&lt;BR /&gt;[CCS last error: mpc83xx: cannot put the target into DEBUG mode ](CCSProtocolPlugin)&lt;BR /&gt;Error: Connect Failed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 29 Sep 2018 10:28:36 GMT</pubDate>
    <dc:creator>usingbothmuxand</dc:creator>
    <dc:date>2018-09-29T10:28:36Z</dc:date>
    <item>
      <title>MPC8309 Custom board with NandFlash</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MPC8309-Custom-board-with-NandFlash/m-p/808103#M7035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we have designed a custom board based on MPC8309. we are targeting NAND flash based Uboot and application.&lt;/P&gt;&lt;P&gt;we have configured reset configuration words nand flash small page. based on that i have configured calculated RCW.&lt;/P&gt;&lt;P&gt;as it is a bare board the RCW are not found in the flash memory. instead i have followed the procedure as suggested in PA arch manual for loading RCW in bare boards. i am using the default files of MPCTWR and changing only the RCWLR and RCWHR values in the MPC8309TWR_HRCW_JTAG.txt present in jtag chains. i have modified the value as below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;8309 (1 1) (2 0x42040003) (3 0xA4140000) (what actually is 2 and 3 here ?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when following the procedure as suggested by NXP i am seeing the following error.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(Targeting_PA_Processors.pdf to use CodeWarrior JTAG&amp;nbsp;configuration file to override RCW on the target board. )&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error message: mpc83xx: cannot put the target into DEBUG mode.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there anything to be modified for NAND based boot? what needs to be done to properly load the RCW via the debugger&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Akhilesh&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2018 09:11:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MPC8309-Custom-board-with-NandFlash/m-p/808103#M7035</guid>
      <dc:creator>usingbothmuxand</dc:creator>
      <dc:date>2018-09-28T09:11:17Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8309 Custom board with NandFlash</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MPC8309-Custom-board-with-NandFlash/m-p/808104#M7036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i am seeing the following error&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Performing target initialization ...&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;Error:&amp;nbsp; Connect Failed.&lt;BR /&gt;Failed to reset the target&lt;BR /&gt;[CCS last error: mpc83xx: cannot put the target into DEBUG mode ](CCSProtocolPlugin)&lt;BR /&gt;Error: Connect Failed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Sep 2018 10:28:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MPC8309-Custom-board-with-NandFlash/m-p/808104#M7036</guid>
      <dc:creator>usingbothmuxand</dc:creator>
      <dc:date>2018-09-29T10:28:36Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8309 Custom board with NandFlash</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MPC8309-Custom-board-with-NandFlash/m-p/808105#M7037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="27768" data-username="usingbothmuxandnon_mux" href="https://community.nxp.com/people/usingbothmuxandnon_mux"&gt;Akhilesh Chidare&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please configure CFG_RESET_SOURCE[0:3] to configure the processor to use the hard-coded RCW, please refer to "4.3.3.3 Default Reset Configuration Words" for details, then connect CodeWarrior to the target board.&lt;/P&gt;&lt;P&gt;If this problem remains, please check JTAG interface hardware design, please refer to page 5 in the attached ppt to check the hardware design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If further assistance is needed, please enable CCS log in CodeWarrior IDE and copy this log to me to do more investigation, please refer to the following procedure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please &lt;SPAN&gt;&lt;STRONG&gt;enable&lt;/STRONG&gt;&lt;/SPAN&gt; CCS log from "Run-&amp;gt;Debug Configurations-&amp;gt;&amp;lt;project&amp;gt;-core0_RAM_-Connect(Download)-&amp;gt;Edit...-&amp;gt;Advanced-&amp;gt;Advanced CCS setting-&amp;gt;Enable logging", and connect to the target from "Run-&amp;gt;Debug Configurations-&amp;gt;&amp;lt;project&amp;gt;-core0_RAM_-Connect(Download)-&amp;gt;Debug”, the CCS log will be displayed in the console panel in CodeWarrior IDE. If the CCS log in the console is truncated, please enlarge the console buffer from Window-&amp;gt;Preferences-&amp;gt;Run/Debug-&amp;gt;Console-&amp;gt;uncheck "Limit console output".&lt;/P&gt;&lt;P&gt;(Please open the console panel from Window-&amp;gt;Show View-&amp;gt;Console, and if nothing displayed, please choose the correct session on the right top icon in the panel.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Oct 2018 13:48:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MPC8309-Custom-board-with-NandFlash/m-p/808105#M7037</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2018-10-20T13:48:04Z</dc:date>
    </item>
  </channel>
</rss>