<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックCodeWarrior &amp; Debugger: Unable to open specified port</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-Debugger-Unable-to-open-specified-port/m-p/800149#M6994</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a DEMO9S12XDT board and a PE USB Multilink programmer (the red one). Programming the target under native Win7 works fine with CodeWarrior 5.1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I run the same SW and same HW under Linux-&amp;gt;VirtualBox-&amp;gt;Win7, running the debug command opens the True-Time Simulator &amp;amp; Real-Time Debugger window and then another window entitled "P&amp;amp;E HC(S)12 Connection Manager" where Interface and Port are correctly listed at first. If I press the Connect button in Connection Manager, it replaces the port info with "Undetected. Disconnect/Connect USB cable. Click Refresh List." This does not help. The Command sub-window in the Debugger program has a message "Unable to open specified port".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see the USB Multilink 2.0 entry in Control panel Peripheral devices. The programmer has both blue and yellow LEDs illuminated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone managed to get this working under VirtualBox?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Jul 2018 21:38:14 GMT</pubDate>
    <dc:creator>baltazarbalthos</dc:creator>
    <dc:date>2018-07-30T21:38:14Z</dc:date>
    <item>
      <title>CodeWarrior &amp; Debugger: Unable to open specified port</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-Debugger-Unable-to-open-specified-port/m-p/800149#M6994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a DEMO9S12XDT board and a PE USB Multilink programmer (the red one). Programming the target under native Win7 works fine with CodeWarrior 5.1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I run the same SW and same HW under Linux-&amp;gt;VirtualBox-&amp;gt;Win7, running the debug command opens the True-Time Simulator &amp;amp; Real-Time Debugger window and then another window entitled "P&amp;amp;E HC(S)12 Connection Manager" where Interface and Port are correctly listed at first. If I press the Connect button in Connection Manager, it replaces the port info with "Undetected. Disconnect/Connect USB cable. Click Refresh List." This does not help. The Command sub-window in the Debugger program has a message "Unable to open specified port".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see the USB Multilink 2.0 entry in Control panel Peripheral devices. The programmer has both blue and yellow LEDs illuminated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone managed to get this working under VirtualBox?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jul 2018 21:38:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-Debugger-Unable-to-open-specified-port/m-p/800149#M6994</guid>
      <dc:creator>baltazarbalthos</dc:creator>
      <dc:date>2018-07-30T21:38:14Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior &amp; Debugger: Unable to open specified port</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-Debugger-Unable-to-open-specified-port/m-p/800150#M6995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I find a discussion about install CW on virtual box.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/344923"&gt;usb connection fail&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;anyway installing CW on virtual box is not recommended. please install CW on our recommend windows platform.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jennie Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Aug 2018 08:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-Debugger-Unable-to-open-specified-port/m-p/800150#M6995</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2018-08-03T08:56:01Z</dc:date>
    </item>
  </channel>
</rss>