<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックSecure boot activation onto LS1043</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Secure-boot-activation-onto-LS1043/m-p/778965#M6829</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have to activate Secure Boot functionnality onto CPU board with ls1043.&lt;/P&gt;&lt;P&gt;To do this, I have to write &lt;SPAN class=""&gt;OTPMK registers&lt;/SPAN&gt;. I see that every body use CodeWarrior IDE including ccs tools to do this with a JTAG link.&lt;/P&gt;&lt;P&gt;Is there an another solution ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Feb 2018 15:56:55 GMT</pubDate>
    <dc:creator>sergepayre</dc:creator>
    <dc:date>2018-02-01T15:56:55Z</dc:date>
    <item>
      <title>Secure boot activation onto LS1043</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Secure-boot-activation-onto-LS1043/m-p/778965#M6829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have to activate Secure Boot functionnality onto CPU board with ls1043.&lt;/P&gt;&lt;P&gt;To do this, I have to write &lt;SPAN class=""&gt;OTPMK registers&lt;/SPAN&gt;. I see that every body use CodeWarrior IDE including ccs tools to do this with a JTAG link.&lt;/P&gt;&lt;P&gt;Is there an another solution ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Feb 2018 15:56:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Secure-boot-activation-onto-LS1043/m-p/778965#M6829</guid>
      <dc:creator>sergepayre</dc:creator>
      <dc:date>2018-02-01T15:56:55Z</dc:date>
    </item>
    <item>
      <title>Re: Secure boot activation onto LS1043</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Secure-boot-activation-onto-LS1043/m-p/778966#M6830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="308116" data-username="sergepayre" href="https://community.nxp.com/people/sergepayre"&gt;Serge Payre&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could write OTPMK to mirror registers under u-boot prompt, after check OTPMK_ZERO and OTPMK_SYNDROME as 0 in SecMon_HP, check SFP_SVHESR no parity error, please write OTPMK from mirror registers into the fuse array permanently.&lt;/P&gt;&lt;P&gt;Please use u-boot command "mw" and "mm" to write and dump OTPMK&amp;nbsp; related registers.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 25 Feb 2018 12:32:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Secure-boot-activation-onto-LS1043/m-p/778966#M6830</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2018-02-25T12:32:24Z</dc:date>
    </item>
  </channel>
</rss>