<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Eclipse plugins for Codewarrior (10.6) in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Eclipse-plugins-for-Codewarrior-10-6/m-p/775928#M6794</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use CW10.6 for DSC programming. I've recently been customising eclipse builds and found some useful plugins that make life easier, for example hooking up with SVN using subclipse / subversive. However, I can't add the plugins to Codewarrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I then found I need the Eclipse Marketplace installed. I can't add that either. I noticed at this poin there are a few disabled sites in the&amp;nbsp;CodeWarrior sites drop down box.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My questions then are:&lt;/P&gt;&lt;P&gt;1. Is it recommended not&amp;nbsp;to add plugins to Codewarrior 10.6? (or 10.anything?)&lt;/P&gt;&lt;P&gt;2. If it is ok to add in plugins, would this invalidate support / warranty agreements?&lt;/P&gt;&lt;P&gt;3. If it doesn't invalidate support / warranties, how does one go about it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Nov 2017 13:20:08 GMT</pubDate>
    <dc:creator>TurboMan</dc:creator>
    <dc:date>2017-11-14T13:20:08Z</dc:date>
    <item>
      <title>Eclipse plugins for Codewarrior (10.6)</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Eclipse-plugins-for-Codewarrior-10-6/m-p/775928#M6794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use CW10.6 for DSC programming. I've recently been customising eclipse builds and found some useful plugins that make life easier, for example hooking up with SVN using subclipse / subversive. However, I can't add the plugins to Codewarrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I then found I need the Eclipse Marketplace installed. I can't add that either. I noticed at this poin there are a few disabled sites in the&amp;nbsp;CodeWarrior sites drop down box.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My questions then are:&lt;/P&gt;&lt;P&gt;1. Is it recommended not&amp;nbsp;to add plugins to Codewarrior 10.6? (or 10.anything?)&lt;/P&gt;&lt;P&gt;2. If it is ok to add in plugins, would this invalidate support / warranty agreements?&lt;/P&gt;&lt;P&gt;3. If it doesn't invalidate support / warranties, how does one go about it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Nov 2017 13:20:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Eclipse-plugins-for-Codewarrior-10-6/m-p/775928#M6794</guid>
      <dc:creator>TurboMan</dc:creator>
      <dc:date>2017-11-14T13:20:08Z</dc:date>
    </item>
    <item>
      <title>Re: Eclipse plugins for Codewarrior (10.6)</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Eclipse-plugins-for-Codewarrior-10-6/m-p/775929#M6795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;CW10.6 is based on Eclipse 4.2. If the plug in supports Eclipse 4.2, Normally, it can be also installed on CW10.6.&lt;/P&gt;&lt;P&gt;There is already some discussion of how to install SVN on CW10. Please refer:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/301424"&gt;Subversion (SVN) Codewarrior 10&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/382038"&gt;https://community.nxp.com/thread/382038&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Nov 2017 03:43:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Eclipse-plugins-for-Codewarrior-10-6/m-p/775929#M6795</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2017-11-24T03:43:57Z</dc:date>
    </item>
  </channel>
</rss>