<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What is the difference between &amp;quot;ARMv8 v11.2.5 b170927 - Linux&amp;quot; and &amp;quot;Installer: CodeWarrior Networked Applications Linux Hosted-Offline v2017.03&amp;quot;? in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/What-is-the-difference-between-quot-ARMv8-v11-2-5-b170927-Linux/m-p/774341#M6776</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yiping,&lt;/P&gt;&lt;P&gt;In installed updates through CodeWarrior's "Help &amp;gt; Check for Updates" menu&lt;/P&gt;&lt;P&gt;option. Would this have installed the updates in "ARMv8 v11.25 b170927 -&lt;/P&gt;&lt;P&gt;Linux", or do I need to install those separately?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Brett S.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Dec 2017 13:27:17 GMT</pubDate>
    <dc:creator>brettstahlman</dc:creator>
    <dc:date>2017-12-04T13:27:17Z</dc:date>
    <item>
      <title>What is the difference between "ARMv8 v11.2.5 b170927 - Linux" and "Installer: CodeWarrior Networked Applications Linux Hosted-Offline v2017.03"?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/What-is-the-difference-between-quot-ARMv8-v11-2-5-b170927-Linux/m-p/774338#M6773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to download/install the evaluation version of CodeWarrior for use with the&amp;nbsp;LS1012A evaluation board. I've gone to the download page, and I see&amp;nbsp;2 basic packages available for download: one is clearly an "Installer"; the&amp;nbsp;name of the other doesn't give much of a clue as to what it is. Are the packages mutually-exclusive, or are both needed, and if so, for what?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Brett S.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Nov 2017 16:07:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/What-is-the-difference-between-quot-ARMv8-v11-2-5-b170927-Linux/m-p/774338#M6773</guid>
      <dc:creator>brettstahlman</dc:creator>
      <dc:date>2017-11-14T16:07:51Z</dc:date>
    </item>
    <item>
      <title>Re: What is the difference between "ARMv8 v11.2.5 b170927 - Linux" and "Installer: CodeWarrior Networked Applications Linux Hosted-Offline v2017.03"?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/What-is-the-difference-between-quot-ARMv8-v11-2-5-b170927-Linux/m-p/774339#M6774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to figure this out too. &amp;nbsp;I've dowloaded, installed, and been using &lt;STRONG&gt;CodeWarrior Networked Applications Linux Hosted-Offline v2017.03.tar&lt;/STRONG&gt; (dated March, 2017). I also downloaded&amp;nbsp;&lt;STRONG&gt;ARMv8 v11.2.5 b170927 - Linux.zip&lt;/STRONG&gt; which appears to be more recent (September 27, 2017?). &amp;nbsp;The folder structure within the ZIP file doesn't bear any obvious resemblance to the CW installation under /usr/local/Freescale so I'm puzzled if it is an update and, if so, how it is supposed to be used or merged with the CW installation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Nov 2017 18:03:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/What-is-the-difference-between-quot-ARMv8-v11-2-5-b170927-Linux/m-p/774339#M6774</guid>
      <dc:creator>ACGarland</dc:creator>
      <dc:date>2017-11-16T18:03:30Z</dc:date>
    </item>
    <item>
      <title>Re: What is the difference between "ARMv8 v11.2.5 b170927 - Linux" and "Installer: CodeWarrior Networked Applications Linux Hosted-Offline v2017.03"?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/What-is-the-difference-between-quot-ARMv8-v11-2-5-b170927-Linux/m-p/774340#M6775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The file "CodeWarrior Networked Applications Linux Hosted-Offline v2017.03.tar" is the base installation tar ball for CodeWarrior v2017.03(v11.2.3).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The file ARMv8 v11.2.5 b170927 - Linux.zip is the patch release used to update CodeWarrior to the latest version 11.2.5. After install CodeWarrior 2017.03, please install the patch(zip) file in CodeWarrior IDE from Help-&amp;gt;Install New Software-&amp;gt;Add-&amp;gt;Archive, please specify the path of the zip file and follow the installation wizards to install it step by step.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Dec 2017 06:48:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/What-is-the-difference-between-quot-ARMv8-v11-2-5-b170927-Linux/m-p/774340#M6775</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-12-04T06:48:31Z</dc:date>
    </item>
    <item>
      <title>Re: What is the difference between "ARMv8 v11.2.5 b170927 - Linux" and "Installer: CodeWarrior Networked Applications Linux Hosted-Offline v2017.03"?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/What-is-the-difference-between-quot-ARMv8-v11-2-5-b170927-Linux/m-p/774341#M6776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yiping,&lt;/P&gt;&lt;P&gt;In installed updates through CodeWarrior's "Help &amp;gt; Check for Updates" menu&lt;/P&gt;&lt;P&gt;option. Would this have installed the updates in "ARMv8 v11.25 b170927 -&lt;/P&gt;&lt;P&gt;Linux", or do I need to install those separately?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Brett S.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Dec 2017 13:27:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/What-is-the-difference-between-quot-ARMv8-v11-2-5-b170927-Linux/m-p/774341#M6776</guid>
      <dc:creator>brettstahlman</dc:creator>
      <dc:date>2017-12-04T13:27:17Z</dc:date>
    </item>
    <item>
      <title>Re: What is the difference between "ARMv8 v11.2.5 b170927 - Linux" and "Installer: CodeWarrior Networked Applications Linux Hosted-Offline v2017.03"?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/What-is-the-difference-between-quot-ARMv8-v11-2-5-b170927-Linux/m-p/774342#M6777</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Yiping Wang wrote:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After install CodeWarrior 2017.03, please install the patch(zip) file in CodeWarrior IDE from Help-&amp;gt;Install New Software-&amp;gt;Add-&amp;gt;Archive, please specify the path of the zip file and follow the installation wizards to install it step by step.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I was able to add the ZIP file as an archive, but during the install process encounter an error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18863i3505142B1F8142AC/image-size/large?v=v2&amp;amp;px=999" title="Screen Shot 2017-12-08 at 5.15.35 PM.png" alt="Screen Shot 2017-12-08 at 5.15.35 PM.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm assuming this means the patch doesn't successfully get applied? &amp;nbsp;Any idea what this problem may be?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've attached the diagnostic info that was created (as mentioned in the above dialog).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Dec 2017 18:34:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/What-is-the-difference-between-quot-ARMv8-v11-2-5-b170927-Linux/m-p/774342#M6777</guid>
      <dc:creator>ACGarland</dc:creator>
      <dc:date>2017-12-13T18:34:35Z</dc:date>
    </item>
  </channel>
</rss>