<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CW10 &amp; P&amp;E Cyclone FX in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW10-P-E-Cyclone-FX/m-p/766585#M6739</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check community content in the following link: &lt;A _jive_internal="true" href="https://community.nxp.com/message/600009"&gt;https://community.nxp.com/message/600009&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems like there was a similar problem in this community thread and it was solved by choosing the following configuration when creating the project for the FXTH87: select S08-&amp;gt;FXTH8700 Family&amp;gt; FXTH870000.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If this does not solve your case, I would recommend you to add the detailed issue you are facing (including screenshots of the error message) in that same community thread.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 May 2018 16:07:05 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2018-05-01T16:07:05Z</dc:date>
    <item>
      <title>CW10 &amp; P&amp;E Cyclone FX</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW10-P-E-Cyclone-FX/m-p/766584#M6738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;PRE&gt;Operating System: Windows 10 64-bit
- Using CW10 to debug NXP TMPS hardware; specifically the 
FXTH87 TPMS microchip.
- Target is powered via seperate DC power supply; 2.5V, 25mA.
- All latest P&amp;amp;E driver updates are installed. 
- Debugger is visible and is automatically selected in CW10.
- Tried playing with debug configurations, each time recieve the same dialog box with error
stating the target has not been detected.

Has anyone else had a similar issue when using this debugger with CW10?

thanks in advance,

&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2018 10:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW10-P-E-Cyclone-FX/m-p/766584#M6738</guid>
      <dc:creator>silentsam</dc:creator>
      <dc:date>2018-04-25T10:36:40Z</dc:date>
    </item>
    <item>
      <title>Re: CW10 &amp; P&amp;E Cyclone FX</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW10-P-E-Cyclone-FX/m-p/766585#M6739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check community content in the following link: &lt;A _jive_internal="true" href="https://community.nxp.com/message/600009"&gt;https://community.nxp.com/message/600009&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems like there was a similar problem in this community thread and it was solved by choosing the following configuration when creating the project for the FXTH87: select S08-&amp;gt;FXTH8700 Family&amp;gt; FXTH870000.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If this does not solve your case, I would recommend you to add the detailed issue you are facing (including screenshots of the error message) in that same community thread.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 May 2018 16:07:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW10-P-E-Cyclone-FX/m-p/766585#M6739</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2018-05-01T16:07:05Z</dc:date>
    </item>
  </channel>
</rss>