<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Codewarrior debugging, SOPT1 register problem in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-debugging-SOPT1-register-problem/m-p/720661#M6408</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Greg.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your attachment includes part of the source code but not project, so I can't test it.&lt;/P&gt;&lt;P&gt;You mentioned you experienced debugging problem with &lt;SPAN style="color: #222222; background-color: #ffffff; font-size: small;"&gt;SOPT1&amp;nbsp; register.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;One possible reason is that SOPT1 register includes STOPE bit which is to enable stop mode. while stop mode is enabled, we can not debug code normally.&lt;/P&gt;&lt;P&gt;Please check this point.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Oct 2017 06:52:23 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2017-10-30T06:52:23Z</dc:date>
    <item>
      <title>Codewarrior debugging, SOPT1 register problem</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-debugging-SOPT1-register-problem/m-p/720660#M6407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #222222; background-color: #ffffff; font-size: small;"&gt;Hello guys. I'm actually working in Codewarrior&amp;nbsp;v10.6 with a Micro DEMOQE128, and I'm trying to make the drivers of a motor work with the PWM of the micro. The code seems to be quite&amp;nbsp;simple because it only tries to make the drivers work based on a lecture for a proximity sensor, which it's read it with the Mic ADC Converter. At the beginning, it was working fine, but&amp;nbsp; now as sudden as I run the program on the Mic while debugging, I got a problem with the SOPT1 register of the Mic (It stops like it was a breakpoint or some stuff like that), so it is really driving me crazy, because my code it's really short and I've never modified or even open the CPU registers.&amp;nbsp;&lt;/SPAN&gt;&lt;BR style="color: #222222; font-size: small;" /&gt;&lt;SPAN style="color: #222222; background-color: #ffffff; font-size: small;"&gt;Thanks so much in advance, really&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Oct 2017 01:55:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-debugging-SOPT1-register-problem/m-p/720660#M6407</guid>
      <dc:creator>gregspinetti</dc:creator>
      <dc:date>2017-10-26T01:55:26Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior debugging, SOPT1 register problem</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-debugging-SOPT1-register-problem/m-p/720661#M6408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Greg.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your attachment includes part of the source code but not project, so I can't test it.&lt;/P&gt;&lt;P&gt;You mentioned you experienced debugging problem with &lt;SPAN style="color: #222222; background-color: #ffffff; font-size: small;"&gt;SOPT1&amp;nbsp; register.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;One possible reason is that SOPT1 register includes STOPE bit which is to enable stop mode. while stop mode is enabled, we can not debug code normally.&lt;/P&gt;&lt;P&gt;Please check this point.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Oct 2017 06:52:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-debugging-SOPT1-register-problem/m-p/720661#M6408</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2017-10-30T06:52:23Z</dc:date>
    </item>
  </channel>
</rss>