<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Tools中的主题 Add items to ProcessorExpert.prm</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Add-items-to-ProcessorExpert-prm/m-p/708376#M6288</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have used ProcessorExpert to create a S08 application, but I need to add items to the linker file ProcessorExper.pr.m but every time i build the app the file is re-generated without my additions. How can I stop this from happening?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Sep 2017 17:22:35 GMT</pubDate>
    <dc:creator>juliancox</dc:creator>
    <dc:date>2017-09-19T17:22:35Z</dc:date>
    <item>
      <title>Add items to ProcessorExpert.prm</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Add-items-to-ProcessorExpert-prm/m-p/708376#M6288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have used ProcessorExpert to create a S08 application, but I need to add items to the linker file ProcessorExper.pr.m but every time i build the app the file is re-generated without my additions. How can I stop this from happening?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Sep 2017 17:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Add-items-to-ProcessorExpert-prm/m-p/708376#M6288</guid>
      <dc:creator>juliancox</dc:creator>
      <dc:date>2017-09-19T17:22:35Z</dc:date>
    </item>
    <item>
      <title>Re: Add items to ProcessorExpert.prm</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Add-items-to-ProcessorExpert-prm/m-p/708377#M6289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Julian.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In processor expert project, prm file is generated by processor expert by default.&lt;/P&gt;&lt;P&gt;During working with pe project, prm will be overwritten after each code generation.&lt;/P&gt;&lt;P&gt;To avoid prm being overwritten, we need to set pe Build options&amp;nbsp; "Generate PRM file" as "NO". see below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30798iDD35A5513B33D3B1/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Sep 2017 01:47:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Add-items-to-ProcessorExpert-prm/m-p/708377#M6289</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2017-09-20T01:47:53Z</dc:date>
    </item>
  </channel>
</rss>