<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: Ethernet TAP is not supported starting ccs 439</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Ethernet-TAP-is-not-supported-starting-ccs-439/m-p/707813#M6287</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="301905" data-username="shuaiwei" href="https://community.nxp.com/people/shuaiwei"&gt;Shuai Wei&lt;/A&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;First I explain something about Ethernet TAP and CodeWarrior TAP. Ethernet TAP is the old product, only integrates Ethernet port, customers cannot purchase this product now. CodeWarrior TAP is the new product, it integrates both USB and Ethernet ports. &lt;BR /&gt;I believe you are using CodeWarrior TAP with Ethernet connection. So when you use QCVS tool, please specify the connection type as CWTAP with IP address.&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;In addition, please open CCS console and type the following commands to do further validation.&lt;BR /&gt;(bin) 30 % config cc cwtap:192.168.1.250&lt;BR /&gt;(bin) 31 % show cc&lt;BR /&gt;CodeWarrior TAP executable differs from local file.&lt;BR /&gt;CodeWarrior TAP Boot Loader version 1.0.1&lt;BR /&gt;CodeWarrior TAP OS version 1.0.1&lt;BR /&gt;Sending code to CodeWarrior TAP.........done&lt;BR /&gt;Running package script&lt;BR /&gt;0: CodeWarrior TAP (cwtap:92.168.1.250) CC software ver. {0.0}&lt;BR /&gt;(bin) 32 % &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Aug 2017 09:54:36 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2017-08-31T09:54:36Z</dc:date>
    <item>
      <title>Ethernet TAP is not supported starting ccs 439</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Ethernet-TAP-is-not-supported-starting-ccs-439/m-p/707812#M6286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i use QCVS intergred in codewarrior for PA to debug DDR, but the connection through Ethernet TAP doesn't work, and the ccs log is shown as below:&lt;/P&gt;&lt;P&gt;CodeWarrior Connection Server console display active (Tcl8.4.12 / Tk8.4.12)&lt;BR /&gt;Loading CCSAPI Tcl interface (E:/Freescale/CW_PA_v10.5.0/eclipse/Optimization/target-connection/cdde/ccs/bin/ccstcl.dll)...&lt;BR /&gt;Loading Svfburner (E:/Freescale/CW_PA_v10.5.0/eclipse/Optimization/target-connection/cdde/ccs/bin/svfburner.dll)...&lt;BR /&gt;There are no command converters configured&lt;BR /&gt;Server listening on port: 41475&lt;BR /&gt;Server listening on port: 50000&lt;BR /&gt;Clients allowed from all hosts&lt;BR /&gt;No clients denied&lt;BR /&gt;CCSAPI connection #1 accepted from PC-PC at Fri Aug 25 19:31:44 2017&lt;BR /&gt;Ethernet TAP is not supported starting ccs 439&lt;BR /&gt;cannot connect to 192.168.1.250:1087&lt;BR /&gt;Ethernet TAP is not supported starting ccs 439&lt;BR /&gt;cannot connect to 192.168.1.250:1087&lt;BR /&gt;CCSAPI connection #1 from PC-PC closed at Fri Aug 25 19:31:54 2017&lt;BR /&gt;Ethernet TAP is not supported starting ccs 439&lt;BR /&gt;cannot connect to 192.168.1.250:1087&lt;BR /&gt;CCSAPI connection #1 accepted from PC-PC at Fri Aug 25 19:32:55 2017&lt;BR /&gt;Ethernet TAP is not supported starting ccs 439&lt;BR /&gt;cannot connect to 192.168.1.250:1087&lt;BR /&gt;Ethernet TAP is not supported starting ccs 439&lt;BR /&gt;cannot connect to 192.168.1.250:1087&lt;BR /&gt;CCSAPI connection #1 from PC-PC closed at Fri Aug 25 19:33:06 2017&lt;BR /&gt;Ethernet TAP is not supported starting ccs 439&lt;BR /&gt;cannot connect to 192.168.1.250:1087&lt;BR /&gt;CCSAPI connection #1 accepted from PC-PC at Fri Aug 25 19:35:01 2017&lt;BR /&gt;Ethernet TAP is not supported starting ccs 439&lt;BR /&gt;cannot connect to 192.168.1.250:1087&lt;BR /&gt;Ethernet TAP is not supported starting ccs 439&lt;BR /&gt;cannot connect to 192.168.1.250:1087&lt;BR /&gt;CCSAPI connection #1 from PC-PC closed at Fri Aug 25 19:35:11 2017&lt;BR /&gt;Ethernet TAP is not supported starting ccs 439&lt;BR /&gt;cannot connect to 192.168.1.250:1087&lt;BR /&gt;CCSAPI connection #1 accepted from PC-PC at Fri Aug 25 19:35:18 2017&lt;BR /&gt;Ethernet TAP is not supported starting ccs 439&lt;BR /&gt;cannot connect to 192.168.1.250:1087&lt;BR /&gt;Ethernet TAP is not supported starting ccs 439&lt;BR /&gt;cannot connect to 192.168.1.250:1087&lt;BR /&gt;CCSAPI connection #1 from PC-PC closed at Fri Aug 25 19:35:28 2017&lt;BR /&gt;(bin) 2 %&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Aug 2017 12:24:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Ethernet-TAP-is-not-supported-starting-ccs-439/m-p/707812#M6286</guid>
      <dc:creator>shuaiwei</dc:creator>
      <dc:date>2017-08-25T12:24:50Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet TAP is not supported starting ccs 439</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Ethernet-TAP-is-not-supported-starting-ccs-439/m-p/707813#M6287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="301905" data-username="shuaiwei" href="https://community.nxp.com/people/shuaiwei"&gt;Shuai Wei&lt;/A&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;First I explain something about Ethernet TAP and CodeWarrior TAP. Ethernet TAP is the old product, only integrates Ethernet port, customers cannot purchase this product now. CodeWarrior TAP is the new product, it integrates both USB and Ethernet ports. &lt;BR /&gt;I believe you are using CodeWarrior TAP with Ethernet connection. So when you use QCVS tool, please specify the connection type as CWTAP with IP address.&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;In addition, please open CCS console and type the following commands to do further validation.&lt;BR /&gt;(bin) 30 % config cc cwtap:192.168.1.250&lt;BR /&gt;(bin) 31 % show cc&lt;BR /&gt;CodeWarrior TAP executable differs from local file.&lt;BR /&gt;CodeWarrior TAP Boot Loader version 1.0.1&lt;BR /&gt;CodeWarrior TAP OS version 1.0.1&lt;BR /&gt;Sending code to CodeWarrior TAP.........done&lt;BR /&gt;Running package script&lt;BR /&gt;0: CodeWarrior TAP (cwtap:92.168.1.250) CC software ver. {0.0}&lt;BR /&gt;(bin) 32 % &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 09:54:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Ethernet-TAP-is-not-supported-starting-ccs-439/m-p/707813#M6287</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-08-31T09:54:36Z</dc:date>
    </item>
  </channel>
</rss>