<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: Code warrior + USB TAP in Window 10 system can not connect to 56F8013 based board</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-warrior-USB-TAP-in-Window-10-system-can-not-connect-to/m-p/687614#M6128</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;USB tap 4.13 can work with CW10.6.4&amp;nbsp; on 64bit win10 without problem.&lt;/P&gt;&lt;P&gt;Can you please test your usb tap on another computer with other board,if the usb tap is in good condition and not be damaged?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Aug 2017 03:12:37 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2017-08-08T03:12:37Z</dc:date>
    <item>
      <title>Code warrior + USB TAP in Window 10 system can not connect to 56F8013 based board</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-warrior-USB-TAP-in-Window-10-system-can-not-connect-to/m-p/687613#M6127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have installed code warrior v10.6.4 in my laptop with windows 10 system, using USB TAP, when debug, it can not connect to 56F8013 based board. my ccs version is 4.13. it occurs the following:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3043iD81EBD4B9838AACC/image-size/large?v=v2&amp;amp;px=999" title="ccsfigure.png" alt="ccsfigure.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;how can I fix it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Jul 2017 00:32:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-warrior-USB-TAP-in-Window-10-system-can-not-connect-to/m-p/687613#M6127</guid>
      <dc:creator>weikun</dc:creator>
      <dc:date>2017-07-30T00:32:12Z</dc:date>
    </item>
    <item>
      <title>Re: Code warrior + USB TAP in Window 10 system can not connect to 56F8013 based board</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-warrior-USB-TAP-in-Window-10-system-can-not-connect-to/m-p/687614#M6128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;USB tap 4.13 can work with CW10.6.4&amp;nbsp; on 64bit win10 without problem.&lt;/P&gt;&lt;P&gt;Can you please test your usb tap on another computer with other board,if the usb tap is in good condition and not be damaged?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Aug 2017 03:12:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-warrior-USB-TAP-in-Window-10-system-can-not-connect-to/m-p/687614#M6128</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2017-08-08T03:12:37Z</dc:date>
    </item>
  </channel>
</rss>