<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックP</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/P/m-p/299222#M604</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've installed CW 8.7 on a 64bit Win7 machine following instructions found on a post here.&amp;nbsp; The process basically involves copying the CW install folder from an XP machine.&amp;nbsp; What I've found is that the P&amp;amp;E BDM programmer I use to target a 555 won't work.&amp;nbsp; It returns a "Connect Failed" error when I try and program the processor.&amp;nbsp; P&amp;amp;E said that the issue is that the drivers only work on a 32bit OS.&amp;nbsp; I've installed 32 bit Win 7 on another box, but when I try and install code warrior I get an error that says in part "Failed to install the INF file (C:\Windows\inf\windrvr6.inf) Error updating the driver (hwid:*WINDRVR6) with the INF file:&amp;nbsp; The system cannot find the file specified."&amp;nbsp; I found a posting here that suggested updating the P&amp;amp;E drivers (I did) and also plugging in the USB device so that it installs. I continue to get the same error.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I followed the instructions for 64 bit Win 7 and have CW running, but I still get the connect error.&amp;nbsp; Can anybody give me some guidance on how to get the BDM programmer working with this version of CW running on Win7?&amp;nbsp; There are some other tools that require this version of CW.&amp;nbsp; Thanks, John.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Apr 2014 18:18:18 GMT</pubDate>
    <dc:creator>johndzielski</dc:creator>
    <dc:date>2014-04-17T18:18:18Z</dc:date>
    <item>
      <title>P</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/P/m-p/299222#M604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've installed CW 8.7 on a 64bit Win7 machine following instructions found on a post here.&amp;nbsp; The process basically involves copying the CW install folder from an XP machine.&amp;nbsp; What I've found is that the P&amp;amp;E BDM programmer I use to target a 555 won't work.&amp;nbsp; It returns a "Connect Failed" error when I try and program the processor.&amp;nbsp; P&amp;amp;E said that the issue is that the drivers only work on a 32bit OS.&amp;nbsp; I've installed 32 bit Win 7 on another box, but when I try and install code warrior I get an error that says in part "Failed to install the INF file (C:\Windows\inf\windrvr6.inf) Error updating the driver (hwid:*WINDRVR6) with the INF file:&amp;nbsp; The system cannot find the file specified."&amp;nbsp; I found a posting here that suggested updating the P&amp;amp;E drivers (I did) and also plugging in the USB device so that it installs. I continue to get the same error.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I followed the instructions for 64 bit Win 7 and have CW running, but I still get the connect error.&amp;nbsp; Can anybody give me some guidance on how to get the BDM programmer working with this version of CW running on Win7?&amp;nbsp; There are some other tools that require this version of CW.&amp;nbsp; Thanks, John.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Apr 2014 18:18:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/P/m-p/299222#M604</guid>
      <dc:creator>johndzielski</dc:creator>
      <dc:date>2014-04-17T18:18:18Z</dc:date>
    </item>
    <item>
      <title>Re: P</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/P/m-p/299223#M605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately CodeWarrior for MPC5xx V8.7 is not working on Win 7. It is a 32-bit application. Please view the note on its webpage:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MPC5XX"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MPC5XX&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We recommend to use Windows 2000, Windows XP/Vista (32-bit).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are the official OS supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this time there is no plan for a new version supporting Win 7.&lt;/P&gt;&lt;P&gt;I know a few customers are successfully using CW8.7 on Windows 7, they download the newest 64-Bit-Drivers from P&amp;amp;E for the Multilink-Device, and update some dll's with it.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Nov 2014 11:23:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/P/m-p/299223#M605</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2014-11-06T11:23:02Z</dc:date>
    </item>
  </channel>
</rss>