<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Firmware update required in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Firmware-update-required/m-p/298338#M588</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to connect to a target system which is based on p2020 via CW-TAP and using CW- IDE, but I am getting the following error:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Error launching Myp2020_project-core00_RAM_P2020_Download&lt;/P&gt;&lt;P&gt;CCSProtocolPlugin : Could not connect to the probe (or other debug link)&lt;/P&gt;&lt;P&gt;[CCS last error: Firmware update required ]&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119797i4CC40F9A7A18037A/image-size/large?v=v2&amp;amp;px=999" title="11762_11762.png" alt="11762_11762.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44001iE222CDB59FD6769F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did update the firmware by connecting to CW-TAP using ccs.exe in win7 and following command, but I am still getting the same error when I connect to CW-TAP in IDE environment:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(bin) 1 % updatecwtap --force 10.92.6.50&lt;/P&gt;&lt;P&gt;10.92.6.50 is running OS version 1.0.1&lt;/P&gt;&lt;P&gt;Update contains OS version 1.0.1&lt;/P&gt;&lt;P&gt;WARNING: Update forced - overriding version check.&lt;/P&gt;&lt;P&gt;WARNING: UPDATING FLASH - DO NOT INTERRUPT!&lt;/P&gt;&lt;P&gt;Sending code to CodeWarrior TAP.........done&lt;/P&gt;&lt;P&gt;Running package script&lt;/P&gt;&lt;P&gt;Erasing kernel partition...&lt;/P&gt;&lt;P&gt;Flashing kernel partition...&lt;/P&gt;&lt;P&gt;Erasing root2 partition...&lt;/P&gt;&lt;P&gt;Flashing root2 partition...&lt;/P&gt;&lt;P&gt;Activating root2&lt;/P&gt;&lt;P&gt;Update completed; rebooting.&lt;/P&gt;&lt;P&gt;Waiting for reboot...&lt;/P&gt;&lt;P&gt;10.92.6.50 is running Boot Loader version 0.9.2&lt;/P&gt;&lt;P&gt;Update contains Boot Loader version 0.9.2&lt;/P&gt;&lt;P&gt;WARNING: Update forced - overriding version check.&lt;/P&gt;&lt;P&gt;WARNING: UPDATING FLASH - DO NOT INTERRUPT!&lt;/P&gt;&lt;P&gt;Sending code to CodeWarrior TAP.........done&lt;/P&gt;&lt;P&gt;Running package script&lt;/P&gt;&lt;P&gt;Erasing uboot partition...&lt;/P&gt;&lt;P&gt;Flashing uboot partition...&lt;/P&gt;&lt;P&gt;Update completed; rebooting.&lt;/P&gt;&lt;P&gt;Waiting for reboot...&lt;/P&gt;&lt;P&gt;All updates completed successfully.&lt;/P&gt;&lt;P&gt;(bin) 2 % updatecwtap 10.92.6.50&lt;/P&gt;&lt;P&gt;10.92.6.50 is running OS version 1.0.1&lt;/P&gt;&lt;P&gt;Update contains OS version 1.0.1&lt;/P&gt;&lt;P&gt;No update needed (use '--force' to reinstall).&lt;/P&gt;&lt;P&gt;10.92.6.50 is running Boot Loader version 0.9.2&lt;/P&gt;&lt;P&gt;Update contains Boot Loader version 0.9.2&lt;/P&gt;&lt;P&gt;No update needed (use '--force' to reinstall).&lt;/P&gt;&lt;P&gt;All updates completed successfully.&lt;/P&gt;&lt;P&gt;(bin) 3 %&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 May 2014 13:00:05 GMT</pubDate>
    <dc:creator>alikobari</dc:creator>
    <dc:date>2014-05-15T13:00:05Z</dc:date>
    <item>
      <title>Firmware update required</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Firmware-update-required/m-p/298338#M588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to connect to a target system which is based on p2020 via CW-TAP and using CW- IDE, but I am getting the following error:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Error launching Myp2020_project-core00_RAM_P2020_Download&lt;/P&gt;&lt;P&gt;CCSProtocolPlugin : Could not connect to the probe (or other debug link)&lt;/P&gt;&lt;P&gt;[CCS last error: Firmware update required ]&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119797i4CC40F9A7A18037A/image-size/large?v=v2&amp;amp;px=999" title="11762_11762.png" alt="11762_11762.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44001iE222CDB59FD6769F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did update the firmware by connecting to CW-TAP using ccs.exe in win7 and following command, but I am still getting the same error when I connect to CW-TAP in IDE environment:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(bin) 1 % updatecwtap --force 10.92.6.50&lt;/P&gt;&lt;P&gt;10.92.6.50 is running OS version 1.0.1&lt;/P&gt;&lt;P&gt;Update contains OS version 1.0.1&lt;/P&gt;&lt;P&gt;WARNING: Update forced - overriding version check.&lt;/P&gt;&lt;P&gt;WARNING: UPDATING FLASH - DO NOT INTERRUPT!&lt;/P&gt;&lt;P&gt;Sending code to CodeWarrior TAP.........done&lt;/P&gt;&lt;P&gt;Running package script&lt;/P&gt;&lt;P&gt;Erasing kernel partition...&lt;/P&gt;&lt;P&gt;Flashing kernel partition...&lt;/P&gt;&lt;P&gt;Erasing root2 partition...&lt;/P&gt;&lt;P&gt;Flashing root2 partition...&lt;/P&gt;&lt;P&gt;Activating root2&lt;/P&gt;&lt;P&gt;Update completed; rebooting.&lt;/P&gt;&lt;P&gt;Waiting for reboot...&lt;/P&gt;&lt;P&gt;10.92.6.50 is running Boot Loader version 0.9.2&lt;/P&gt;&lt;P&gt;Update contains Boot Loader version 0.9.2&lt;/P&gt;&lt;P&gt;WARNING: Update forced - overriding version check.&lt;/P&gt;&lt;P&gt;WARNING: UPDATING FLASH - DO NOT INTERRUPT!&lt;/P&gt;&lt;P&gt;Sending code to CodeWarrior TAP.........done&lt;/P&gt;&lt;P&gt;Running package script&lt;/P&gt;&lt;P&gt;Erasing uboot partition...&lt;/P&gt;&lt;P&gt;Flashing uboot partition...&lt;/P&gt;&lt;P&gt;Update completed; rebooting.&lt;/P&gt;&lt;P&gt;Waiting for reboot...&lt;/P&gt;&lt;P&gt;All updates completed successfully.&lt;/P&gt;&lt;P&gt;(bin) 2 % updatecwtap 10.92.6.50&lt;/P&gt;&lt;P&gt;10.92.6.50 is running OS version 1.0.1&lt;/P&gt;&lt;P&gt;Update contains OS version 1.0.1&lt;/P&gt;&lt;P&gt;No update needed (use '--force' to reinstall).&lt;/P&gt;&lt;P&gt;10.92.6.50 is running Boot Loader version 0.9.2&lt;/P&gt;&lt;P&gt;Update contains Boot Loader version 0.9.2&lt;/P&gt;&lt;P&gt;No update needed (use '--force' to reinstall).&lt;/P&gt;&lt;P&gt;All updates completed successfully.&lt;/P&gt;&lt;P&gt;(bin) 3 %&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 May 2014 13:00:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Firmware-update-required/m-p/298338#M588</guid>
      <dc:creator>alikobari</dc:creator>
      <dc:date>2014-05-15T13:00:05Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware update required</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Firmware-update-required/m-p/298339#M589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your post, however please consider moving it to the right community place (e.g. &lt;A href="https://community.nxp.com/space/2020"&gt;CodeWarrior Development Tools&lt;/A&gt; or&amp;nbsp;&amp;nbsp; &lt;A _jive_internal="true" class="jivecontainerTT-hover-container jive-link-community-small" data-containerid="1" data-containertype="14" data-objectid="2009" data-objecttype="14" href="https://community.nxp.com/community/qoriq"&gt;QorIQ Processors &lt;/A&gt;) to get it visible for active members.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For details please see general advice &lt;A _jive_internal="true" data-containerid="2001" data-containertype="14" data-objectid="99909" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99909"&gt;Where to post a Discussion?&lt;/A&gt; (&lt;A _jive_internal="true" data-containerid="2001" data-containertype="14" data-objectid="99909" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99909"&gt;https://community.freescale.com/docs/DOC-99909&lt;/A&gt; )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using Freescale Community. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 May 2014 13:11:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Firmware-update-required/m-p/298339#M589</guid>
      <dc:creator>Wlodek_D_</dc:creator>
      <dc:date>2014-05-15T13:11:16Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware update required</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Firmware-update-required/m-p/298340#M590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Wlodek,&lt;/P&gt;&lt;P&gt;Thank you for your comment, I am new to this community, I will move it right away!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ali,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 May 2014 13:15:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Firmware-update-required/m-p/298340#M590</guid>
      <dc:creator>alikobari</dc:creator>
      <dc:date>2014-05-15T13:15:12Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware update required</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Firmware-update-required/m-p/298341#M591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What's your CodeWarrior version? The latest one on &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW_DSPA" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW_DSPA"&gt;CW_DSPA: CodeWarrior Development Studio v10 for Power Architecture® Technology (Eclipse)&lt;/A&gt; is 10.3.3 and it supports Windows 7 SP1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 May 2014 08:44:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Firmware-update-required/m-p/298341#M591</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2014-05-21T08:44:49Z</dc:date>
    </item>
  </channel>
</rss>