<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Change the DDR2 chips of mpc8309twr development board in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Change-the-DDR2-chips-of-mpc8309twr-development-board/m-p/660696#M5846</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;In our project, I customed a board base on&amp;nbsp;mpc8309twr development board. Because the&amp;nbsp;Hynix H5PS5162FFR DDR2 chip on&amp;nbsp;&lt;SPAN&gt;mpc8309twr development board does not produce now, we need change the chip. We choose the&amp;nbsp;Micron MT47H32M16 to replace the&amp;nbsp;H5PS5162FFR (work in 32bits). But the uboot can not work now. So, we want to use the CodeWarrior software program the uboot into board through CodeWarrior Tap. I changed the ddr configuration part of&amp;nbsp;8309TWR_init_core.tcl file ,&amp;nbsp;but it still does not work. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The&amp;nbsp;CodeWarrior software print :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Downloading Flash Device Driver ... &lt;BR /&gt; Reading flash ID .......&lt;BR /&gt;Error: The algorithm was not able to run on the target or the flash is not configured properly.&lt;BR /&gt;Error: Getting flash ID failed&lt;BR /&gt;Error: The algorithm was not able to run on the target or the flash is not configured properly.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;How to configure the&amp;nbsp;&lt;SPAN&gt;ddr configuration part of&amp;nbsp;8309TWR_init_core.tcl file ?&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Any help will be appreciated！&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337787"&gt;8309TWR_init_core.tcl.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Jan 2017 02:56:01 GMT</pubDate>
    <dc:creator>lijiankun198</dc:creator>
    <dc:date>2017-01-05T02:56:01Z</dc:date>
    <item>
      <title>Change the DDR2 chips of mpc8309twr development board</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Change-the-DDR2-chips-of-mpc8309twr-development-board/m-p/660696#M5846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;In our project, I customed a board base on&amp;nbsp;mpc8309twr development board. Because the&amp;nbsp;Hynix H5PS5162FFR DDR2 chip on&amp;nbsp;&lt;SPAN&gt;mpc8309twr development board does not produce now, we need change the chip. We choose the&amp;nbsp;Micron MT47H32M16 to replace the&amp;nbsp;H5PS5162FFR (work in 32bits). But the uboot can not work now. So, we want to use the CodeWarrior software program the uboot into board through CodeWarrior Tap. I changed the ddr configuration part of&amp;nbsp;8309TWR_init_core.tcl file ,&amp;nbsp;but it still does not work. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The&amp;nbsp;CodeWarrior software print :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Downloading Flash Device Driver ... &lt;BR /&gt; Reading flash ID .......&lt;BR /&gt;Error: The algorithm was not able to run on the target or the flash is not configured properly.&lt;BR /&gt;Error: Getting flash ID failed&lt;BR /&gt;Error: The algorithm was not able to run on the target or the flash is not configured properly.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;How to configure the&amp;nbsp;&lt;SPAN&gt;ddr configuration part of&amp;nbsp;8309TWR_init_core.tcl file ?&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Any help will be appreciated！&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337787"&gt;8309TWR_init_core.tcl.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jan 2017 02:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Change-the-DDR2-chips-of-mpc8309twr-development-board/m-p/660696#M5846</guid>
      <dc:creator>lijiankun198</dc:creator>
      <dc:date>2017-01-05T02:56:01Z</dc:date>
    </item>
    <item>
      <title>Re: Change the DDR2 chips of mpc8309twr development board</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Change-the-DDR2-chips-of-mpc8309twr-development-board/m-p/660697#M5847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, we do not offer ready-to-use target initialization files for any possible customer configurations, because it is not possible to test all customer configurations here, in our labs. Instead, we offer a full set of documentation to let our customers to develop their own custom configurations. To create target initialization file for your custom DDR2 memory configuration, I recommend using the following documents:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.nxp.com/assets/documents/data/en/application-notes/AN3369.pdf?fsrch=1&amp;amp;sr=5&amp;amp;pageNum=1" title="http://cache.nxp.com/assets/documents/data/en/application-notes/AN3369.pdf?fsrch=1&amp;amp;sr=5&amp;amp;pageNum=1"&gt;http://cache.nxp.com/assets/documents/data/en/application-notes/AN3369.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.nxp.com/assets/documents/data/en/application-notes/AN2910.pdf?fsrch=1&amp;amp;sr=4&amp;amp;pageNum=1" title="http://cache.nxp.com/assets/documents/data/en/application-notes/AN2910.pdf?fsrch=1&amp;amp;sr=4&amp;amp;pageNum=1"&gt;http://cache.nxp.com/assets/documents/data/en/application-notes/AN2910.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jan 2017 12:28:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Change-the-DDR2-chips-of-mpc8309twr-development-board/m-p/660697#M5847</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2017-01-31T12:28:33Z</dc:date>
    </item>
  </channel>
</rss>