<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: Codewarrior running slow on Windows 7 64 bit</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-running-slow-on-Windows-7-64-bit/m-p/647735#M5645</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your answers.&amp;nbsp; It looks like the .metadata folder had a problem.&amp;nbsp; After deleting the folder, the debugger became usable again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried to disable OS Awareness flag, but that did not lead to any performance improvements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mike Polyakov&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Dec 2016 16:46:22 GMT</pubDate>
    <dc:creator>mikhailpolyakov</dc:creator>
    <dc:date>2016-12-29T16:46:22Z</dc:date>
    <item>
      <title>Codewarrior running slow on Windows 7 64 bit</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-running-slow-on-Windows-7-64-bit/m-p/647733#M5643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to debug K65 with MQX application in CodeWarrior 10.7.&amp;nbsp; I have a professional license.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Every time I set a break point, it takes over 30 seconds for the windows to settle after it hits the break point.&amp;nbsp;&amp;nbsp; Then, when I try to step through the code, it may take a couple of minutes to go from one statement to the next.&amp;nbsp; I'm running on 1 Windows 7 64 bit machine with 8 GBytes of RAM, so memory is not a problem.&amp;nbsp; Are there any settings I need to check?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Dec 2016 21:51:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-running-slow-on-Windows-7-64-bit/m-p/647733#M5643</guid>
      <dc:creator>mikhailpolyakov</dc:creator>
      <dc:date>2016-12-28T21:51:41Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior running slow on Windows 7 64 bit</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-running-slow-on-Windows-7-64-bit/m-p/647734#M5644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Here is some questions:&lt;/P&gt;&lt;P&gt;- Is this problem is for a specific project or a common issue for all project? how the debugger works if you create a new project with wizard?&lt;/P&gt;&lt;P&gt;- To identify if the problem is because of MQX OS Awareness. please set Target OS as "None", then see how the debug works?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3638i45AB834696F6CFE0/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- what board do you work with? FRDM or TWR board? I may suggest you update the debug port firmware and see how it works?&lt;/P&gt;&lt;P&gt;- backup current workspace .metadata folder then remove it from your workspace. test how debug works?&lt;/P&gt;&lt;P&gt;- if all above can not change anything, try reinstall CW. then test again. How does debug work?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Dec 2016 06:56:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-running-slow-on-Windows-7-64-bit/m-p/647734#M5644</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-12-29T06:56:50Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior running slow on Windows 7 64 bit</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-running-slow-on-Windows-7-64-bit/m-p/647735#M5645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your answers.&amp;nbsp; It looks like the .metadata folder had a problem.&amp;nbsp; After deleting the folder, the debugger became usable again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried to disable OS Awareness flag, but that did not lead to any performance improvements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mike Polyakov&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Dec 2016 16:46:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-running-slow-on-Windows-7-64-bit/m-p/647735#M5645</guid>
      <dc:creator>mikhailpolyakov</dc:creator>
      <dc:date>2016-12-29T16:46:22Z</dc:date>
    </item>
  </channel>
</rss>