<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRunning multiple MCUs from same PC</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Running-multiple-MCUs-from-same-PC/m-p/647322#M5638</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have two TRK-KEA128 devices and I would like to be able to power them through the same PC, but potentially be able to run separate programs on them. For instance, one would be loaded with a "receive" program and the other with a "send" program. Is there a way to do this without having to unplug the devices?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Tyler&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Jan 2017 17:11:19 GMT</pubDate>
    <dc:creator>tylertrigg</dc:creator>
    <dc:date>2017-01-26T17:11:19Z</dc:date>
    <item>
      <title>Running multiple MCUs from same PC</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Running-multiple-MCUs-from-same-PC/m-p/647322#M5638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have two TRK-KEA128 devices and I would like to be able to power them through the same PC, but potentially be able to run separate programs on them. For instance, one would be loaded with a "receive" program and the other with a "send" program. Is there a way to do this without having to unplug the devices?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Tyler&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jan 2017 17:11:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Running-multiple-MCUs-from-same-PC/m-p/647322#M5638</guid>
      <dc:creator>tylertrigg</dc:creator>
      <dc:date>2017-01-26T17:11:19Z</dc:date>
    </item>
    <item>
      <title>Re: Running multiple MCUs from same PC</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Running-multiple-MCUs-from-same-PC/m-p/647323#M5639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you talking about being able to debug both at the same time from CodeWarrior? &amp;nbsp;I've done that, but I haven't tried with OpenSDA, just P&amp;amp;E Cyclones or Multilinks, I think. &amp;nbsp;They show up as separate debug connections.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 Jan 2017 03:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Running-multiple-MCUs-from-same-PC/m-p/647323#M5639</guid>
      <dc:creator>scottm</dc:creator>
      <dc:date>2017-01-29T03:07:20Z</dc:date>
    </item>
    <item>
      <title>Re: Running multiple MCUs from same PC</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Running-multiple-MCUs-from-same-PC/m-p/647324#M5640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have debugged multiple boards from CodeWarrior from a single IDE, including OpenSDA (which same for P&amp;amp;E): &lt;A class="link-titled" href="https://mcuoneclipse.com/2014/01/07/debugging-the-same-project-multiple-times-in-parallel-with-eclipse/" title="https://mcuoneclipse.com/2014/01/07/debugging-the-same-project-multiple-times-in-parallel-with-eclipse/"&gt;Debugging the same Project Multiple Times in Parallel with Eclipse | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The only think to care about is the USB ID: it might change depending on the order and port you plug it in to the host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 Jan 2017 06:49:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Running-multiple-MCUs-from-same-PC/m-p/647324#M5640</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-01-29T06:49:00Z</dc:date>
    </item>
  </channel>
</rss>