<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How do I use gdb to control the CWTAP? in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-do-I-use-gdb-to-control-the-CWTAP/m-p/631099#M5413</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I ordered the CWTAP to send gdb commands to my target system.&amp;nbsp; I could not find any documentation on using gdb with the CWTAP; however, there is a nice video online showing that this is the intended design.&amp;nbsp; How do I send commands from my (gdb) shell to the CWTAP?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've connected my host computer to the CWTAP which I've assigned a static IP of 192.168.1.2.&amp;nbsp; I can ping the CWTAP, so I have a valid IP connection. The CWTAP manual states that gdb uses port 2345.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;From the (gdb) shell I tried the command:&lt;/P&gt;&lt;P&gt;(gdb) target remote 192.168.1.2:2345&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However there was no response and the command timed out.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Oct 2016 20:26:43 GMT</pubDate>
    <dc:creator>jeffhodges</dc:creator>
    <dc:date>2016-10-12T20:26:43Z</dc:date>
    <item>
      <title>How do I use gdb to control the CWTAP?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-do-I-use-gdb-to-control-the-CWTAP/m-p/631099#M5413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I ordered the CWTAP to send gdb commands to my target system.&amp;nbsp; I could not find any documentation on using gdb with the CWTAP; however, there is a nice video online showing that this is the intended design.&amp;nbsp; How do I send commands from my (gdb) shell to the CWTAP?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've connected my host computer to the CWTAP which I've assigned a static IP of 192.168.1.2.&amp;nbsp; I can ping the CWTAP, so I have a valid IP connection. The CWTAP manual states that gdb uses port 2345.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;From the (gdb) shell I tried the command:&lt;/P&gt;&lt;P&gt;(gdb) target remote 192.168.1.2:2345&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However there was no response and the command timed out.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 20:26:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-do-I-use-gdb-to-control-the-CWTAP/m-p/631099#M5413</guid>
      <dc:creator>jeffhodges</dc:creator>
      <dc:date>2016-10-12T20:26:43Z</dc:date>
    </item>
    <item>
      <title>Re: How do I use gdb to control the CWTAP?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-do-I-use-gdb-to-control-the-CWTAP/m-p/631100#M5414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CWTAP doesn't include a gdb server that allow you to control the board. Communication with CWTAP is done using ccs. Starting with CodeWarrior for ARMv8, gdb connection is possible but only using gta, which know to "transform" gdb commands to ccs commands.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There was an intention to move the gdb sevrer on CWTAP, but the project is obsolete.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 06:12:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-do-I-use-gdb-to-control-the-CWTAP/m-p/631100#M5414</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2016-10-13T06:12:53Z</dc:date>
    </item>
  </channel>
</rss>