<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: When I use CodeWarrior8.8 to connect to the target board (mpc8377), there are the following errors: in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630934#M5408</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;flash&amp;nbsp;&lt;/SPAN&gt;programming problems still exist!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Oct 2016 06:58:52 GMT</pubDate>
    <dc:creator>李鹏斌</dc:creator>
    <dc:date>2016-10-13T06:58:52Z</dc:date>
    <item>
      <title>Re: When I use CodeWarrior8.8 to connect to the target board (mpc8377), there are the following errors:</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630929#M5403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems that there is problem with the following configuration in CodeWarrior initialization file, OR0[AM] should be 1111_1100_0000_0000_0(64M), for details please refer to MPC8377 Reference Manual.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;### CS0 - 512K NorFLASH &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;writemem.l 0xe0005000 0xFC000801 # BR0 base address at 0xFc000000, port size 8 bit, GPCM, valid&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;writemem.l 0xe0005004 0xFFF80FF7 # OR0 512K flash size, 15 w.s., timing relaxed&lt;/EM&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If your problem remains, would you please create a new thread to discuss more about CodeWarrior initialization file porting for your target board?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 05:46:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630929#M5403</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2016-10-13T05:46:35Z</dc:date>
    </item>
    <item>
      <title>Re: When I use CodeWarrior8.8 to connect to the target board (mpc8377), there are the following errors:</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630930#M5404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was set up in accordance with the hardware configuration of the board. I tried to set 1111_1100_0000_0000_0 (64M), or not.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 06:11:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630930#M5404</guid>
      <dc:creator>李鹏斌</dc:creator>
      <dc:date>2016-10-13T06:11:10Z</dc:date>
    </item>
    <item>
      <title>Re: When I use CodeWarrior8.8 to connect to the target board (mpc8377), there are the following errors:</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630931#M5405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try whether it would be helpful to configure 0xe0005004 as 0xFC000FF7&lt;EM&gt;.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 06:30:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630931#M5405</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2016-10-13T06:30:17Z</dc:date>
    </item>
    <item>
      <title>Re: When I use CodeWarrior8.8 to connect to the target board (mpc8377), there are the following errors:</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630932#M5406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried or not!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 06:44:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630932#M5406</guid>
      <dc:creator>李鹏斌</dc:creator>
      <dc:date>2016-10-13T06:44:38Z</dc:date>
    </item>
    <item>
      <title>Re: When I use CodeWarrior8.8 to connect to the target board (mpc8377), there are the following errors:</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630933#M5407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you mean the flash programming problem remains?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 06:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630933#M5407</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2016-10-13T06:55:36Z</dc:date>
    </item>
    <item>
      <title>Re: When I use CodeWarrior8.8 to connect to the target board (mpc8377), there are the following errors:</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630934#M5408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;flash&amp;nbsp;&lt;/SPAN&gt;programming problems still exist!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 06:58:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630934#M5408</guid>
      <dc:creator>李鹏斌</dc:creator>
      <dc:date>2016-10-13T06:58:52Z</dc:date>
    </item>
    <item>
      <title>Re: When I use CodeWarrior8.8 to connect to the target board (mpc8377), there are the following errors:</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630935#M5409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you verified whether there is problem with the DDR controller configuration?&lt;/P&gt;&lt;P&gt;Would you please try whether the sample project can be executed successfully in DDR?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Nov 2016 09:24:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Re-When-I-use-CodeWarrior8-8-to-connect-to-the-target-board/m-p/630935#M5409</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2016-11-03T09:24:24Z</dc:date>
    </item>
  </channel>
</rss>