<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックPort existing code to XGate</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-existing-code-to-XGate/m-p/295604#M535</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I am using the Codewarrior IDE(v5.9 special edition) +Processor Exper (v3.02)t to implement my firmware code.&lt;/P&gt;&lt;P&gt;My current project does not include the XGate support.&lt;/P&gt;&lt;P&gt;Currently I am planning to use XGate to offload some of the interrupt tasks from the main controller. I have not found any application note showing a step by step instructions to port an existing code to a XGate Project. Does anybody have any information on how to do this?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;Huck&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Apr 2014 11:54:47 GMT</pubDate>
    <dc:creator>hucklim</dc:creator>
    <dc:date>2014-04-14T11:54:47Z</dc:date>
    <item>
      <title>Port existing code to XGate</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-existing-code-to-XGate/m-p/295604#M535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I am using the Codewarrior IDE(v5.9 special edition) +Processor Exper (v3.02)t to implement my firmware code.&lt;/P&gt;&lt;P&gt;My current project does not include the XGate support.&lt;/P&gt;&lt;P&gt;Currently I am planning to use XGate to offload some of the interrupt tasks from the main controller. I have not found any application note showing a step by step instructions to port an existing code to a XGate Project. Does anybody have any information on how to do this?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;Huck&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Apr 2014 11:54:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-existing-code-to-XGate/m-p/295604#M535</guid>
      <dc:creator>hucklim</dc:creator>
      <dc:date>2014-04-14T11:54:47Z</dc:date>
    </item>
    <item>
      <title>Re: Port existing code to XGate</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-existing-code-to-XGate/m-p/295605#M536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We support HCS12X derivatives with XGate (including XDP512), but we do not support any code generation for XGate. Currently we do not plan to add support for this.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;We say “processor expert does not support any code generation for XGate”, for instance, processor expert can not be able to generate a prm file that include XGate associated content. So user has to rewrite their own xgate supporting prm file but can’t use pe generated prm.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Another example is that pe also can not generate xgate supported vector table, etc. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;thus it loose some of the major advantages of pe. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;This is the reason that if you make a project with XGATE the Proc.Exp. option does not exist.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;in practice, we don’t recommend user use processor expert and xgate together in one project. In practice, we only have sample code that use xgate or&amp;nbsp; pe only but never use them together. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you want add xgate support to processor expert anyway, I ever figure out a solution:&lt;/P&gt;&lt;P&gt;To add XGATE support to the project, we have to follow the steps below:&lt;BR /&gt; 1.&amp;nbsp;&amp;nbsp; import XGATE lib file: Open the project with CW, in project manager window, right click mouse and select “Add files…”, import ansi_xgi.lib from {CW install directory}\lib\xgatec\lib; if you are using floating support XGATE, you need import ansi_xg.lib instead.&lt;BR /&gt; 2.&amp;nbsp;&amp;nbsp; import xgate header and source file: the simple method is to create a new project with xgate. Then copy xgate.h and xgate.cxgate file from its source folder to the current project folder. Then import this two file into the project.&lt;BR /&gt; 3.&amp;nbsp;&amp;nbsp; press ALT+F7, compiler setting, add -D__FAR_DATA to the command line arguments.&lt;BR /&gt; 4.&amp;nbsp;&amp;nbsp; add #include "xgate.h" in your main file. according to your own need, you could change your prm and C file now.&amp;nbsp; &lt;BR /&gt; 5.&amp;nbsp;&amp;nbsp; in prm file, you need allocate proper memory for xgate. You have to change it manually based on your designed xgate memory allocation. Meanwhile, if you use processor expert, you need disable prm generation in cpu bean instpector. &lt;BR /&gt; 6.&amp;nbsp;&amp;nbsp; how to see xgate code in debugger: press F5 to call debugger, in debugger menu “componnet”, “Open”, “Source” to open a new source file window, in the new window, right click mouse and select “show score”, “xgate”. This window is used to show your current xgate code running state.&lt;BR /&gt; 7.&amp;nbsp;&amp;nbsp; how to save the current debugger window configuration: go to debugger menu “File”, “save configuration”. Thus when you open debugger next time, the layout of the debugger windows will be same.&lt;BR /&gt; &lt;BR /&gt; * Note: I suggest you try the above steps in an empty testing project to familiar with these steps first before you perform it into your own project.&lt;BR /&gt; &lt;BR /&gt; I hope this can help you. Have a nice day!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=================================================&lt;/P&gt;&lt;P&gt;this answer if for you. if it helps, please click on "correct answer " button. thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;ZhangJun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Apr 2014 09:05:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-existing-code-to-XGate/m-p/295605#M536</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2014-04-22T09:05:03Z</dc:date>
    </item>
    <item>
      <title>Re: Port existing code to XGate</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-existing-code-to-XGate/m-p/295606#M537</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jennie,&lt;/P&gt;&lt;P&gt;thanks for your step by step instructions. I will try it out on a test project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours sincerely,&lt;/P&gt;&lt;P&gt;Huck Lim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Apr 2014 10:29:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-existing-code-to-XGate/m-p/295606#M537</guid>
      <dc:creator>hucklim</dc:creator>
      <dc:date>2014-04-22T10:29:37Z</dc:date>
    </item>
    <item>
      <title>Re: Port existing code to XGate</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-existing-code-to-XGate/m-p/295607#M538</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you are welcome!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;ZhangJun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Apr 2014 06:37:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-existing-code-to-XGate/m-p/295607#M538</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2014-04-23T06:37:20Z</dc:date>
    </item>
  </channel>
</rss>