<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re:  Flashing issue in code warrior in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Flashing-issue-in-code-warrior/m-p/623967#M5340</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) could you please check if you have correctly installed an updated PE Micro drivers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Is the project you try to load created in CodeWarrior 10.7? Is the project correctly compiled?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) Have you ever been able to load any project into the microcontroller? Did you try with different chip/board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4) Do you use NXP EVB or your own design? In case you use NXP EVB, is reset LED OFF or ON?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;5) Which PE Micro debugger you use? Universal Multilink FX or some different? In case you have Universal Multilink FX did you disconnect&amp;nbsp; JP10 jumper in debugger?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please write me back these details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Apr 2017 12:58:13 GMT</pubDate>
    <dc:creator>martin_kovar</dc:creator>
    <dc:date>2017-04-20T12:58:13Z</dc:date>
    <item>
      <title>Flashing issue in code warrior</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Flashing-issue-in-code-warrior/m-p/623966#M5339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to flash the code to the controller MPC5604s through the codewarriror ,P&amp;amp;E debugger i am getting&lt;/P&gt;&lt;P&gt;"Failed to resume target process ,Downloading binary to target....."error from debugger window.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I am using codewarrior 10.7.0 version.&lt;/P&gt;&lt;P&gt;Also i have attached the error report pls check and kindly help me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Apr 2017 07:37:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Flashing-issue-in-code-warrior/m-p/623966#M5339</guid>
      <dc:creator>mhogun</dc:creator>
      <dc:date>2017-04-19T07:37:29Z</dc:date>
    </item>
    <item>
      <title>Re:  Flashing issue in code warrior</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Flashing-issue-in-code-warrior/m-p/623967#M5340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) could you please check if you have correctly installed an updated PE Micro drivers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Is the project you try to load created in CodeWarrior 10.7? Is the project correctly compiled?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) Have you ever been able to load any project into the microcontroller? Did you try with different chip/board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4) Do you use NXP EVB or your own design? In case you use NXP EVB, is reset LED OFF or ON?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;5) Which PE Micro debugger you use? Universal Multilink FX or some different? In case you have Universal Multilink FX did you disconnect&amp;nbsp; JP10 jumper in debugger?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please write me back these details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Apr 2017 12:58:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Flashing-issue-in-code-warrior/m-p/623967#M5340</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2017-04-20T12:58:13Z</dc:date>
    </item>
  </channel>
</rss>