<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックCommand converter configuration.</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-converter-configuration/m-p/618780#M5250</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;I'm trying to use a codewarrior USB utap on windows 10.&lt;/P&gt;&lt;P&gt;When I open the CCS.exe and&amp;nbsp;type "show cc" I get the message:&lt;/P&gt;&lt;P&gt;"There are no command converters configured".&lt;/P&gt;&lt;P&gt;I type "config cc utap" and now when I try "show cc" I get:&lt;/P&gt;&lt;P&gt;"0: USB TAP (JTAG) (utap) CC software ver. {1.3}"&lt;/P&gt;&lt;P&gt;as expected, and everything is working as it should.&lt;/P&gt;&lt;P&gt;However, if the computer is restarted, sleeps or CCS.exe is run again, I'm back to square one.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way I can make sure it retains its configuration?&lt;/P&gt;&lt;P&gt;Appreciate any help or suggestions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Sep 2016 11:39:45 GMT</pubDate>
    <dc:creator>fredriklund</dc:creator>
    <dc:date>2016-09-14T11:39:45Z</dc:date>
    <item>
      <title>Command converter configuration.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-converter-configuration/m-p/618780#M5250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;I'm trying to use a codewarrior USB utap on windows 10.&lt;/P&gt;&lt;P&gt;When I open the CCS.exe and&amp;nbsp;type "show cc" I get the message:&lt;/P&gt;&lt;P&gt;"There are no command converters configured".&lt;/P&gt;&lt;P&gt;I type "config cc utap" and now when I try "show cc" I get:&lt;/P&gt;&lt;P&gt;"0: USB TAP (JTAG) (utap) CC software ver. {1.3}"&lt;/P&gt;&lt;P&gt;as expected, and everything is working as it should.&lt;/P&gt;&lt;P&gt;However, if the computer is restarted, sleeps or CCS.exe is run again, I'm back to square one.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way I can make sure it retains its configuration?&lt;/P&gt;&lt;P&gt;Appreciate any help or suggestions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Sep 2016 11:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-converter-configuration/m-p/618780#M5250</guid>
      <dc:creator>fredriklund</dc:creator>
      <dc:date>2016-09-14T11:39:45Z</dc:date>
    </item>
    <item>
      <title>Re: Command converter configuration.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-converter-configuration/m-p/618781#M5251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;About 5 minutes after posting I found the answer.&lt;/P&gt;&lt;P&gt;After getting the right configuration I typed "config save".&lt;/P&gt;&lt;P&gt;Now it works even after a restart.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Sep 2016 11:47:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Command-converter-configuration/m-p/618781#M5251</guid>
      <dc:creator>fredriklund</dc:creator>
      <dc:date>2016-09-14T11:47:08Z</dc:date>
    </item>
  </channel>
</rss>