<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is there a demo/example PCIe setup in CodeWarrior for the T1040RDB processor?  I am trying to perform a PCIe transfer from T1040 to a microsemi/actel FPGA and I could use some help setting up CodeWarrior to accomplish this task.  If a design already exist in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-there-a-demo-example-PCIe-setup-in-CodeWarrior-for-the/m-p/618068#M5231</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am looking for an example PCIe design in CodeWarrior that I can use to interface with an FPGA. &amp;nbsp;I am trying to perform writes and reads to FPGA registers as well as be able to DMA from FPGA into T1040RDB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 08 Oct 2016 18:09:38 GMT</pubDate>
    <dc:creator>kirkpatrickburk</dc:creator>
    <dc:date>2016-10-08T18:09:38Z</dc:date>
    <item>
      <title>Is there a demo/example PCIe setup in CodeWarrior for the T1040RDB processor?  I am trying to perform a PCIe transfer from T1040 to a microsemi/actel FPGA and I could use some help setting up CodeWarrior to accomplish this task.  If a design already exist</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-there-a-demo-example-PCIe-setup-in-CodeWarrior-for-the/m-p/618068#M5231</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am looking for an example PCIe design in CodeWarrior that I can use to interface with an FPGA. &amp;nbsp;I am trying to perform writes and reads to FPGA registers as well as be able to DMA from FPGA into T1040RDB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Oct 2016 18:09:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-there-a-demo-example-PCIe-setup-in-CodeWarrior-for-the/m-p/618068#M5231</guid>
      <dc:creator>kirkpatrickburk</dc:creator>
      <dc:date>2016-10-08T18:09:38Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a demo/example PCIe setup in CodeWarrior for the T1040RDB processor?  I am trying to perform a PCIe transfer from T1040 to a microsemi/actel FPGA and I could use some help setting up CodeWarrior to accomplish this task.  If a design already e</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-there-a-demo-example-PCIe-setup-in-CodeWarrior-for-the/m-p/618069#M5232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="287950" data-username="kirkpatrickburke" href="https://community.nxp.com/people/kirkpatrickburke"&gt;Kirkpatrick Burke&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As we discussed in the service requests, I suggest you refer to u-boot source code to configure your target.&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;For LAW and outbound windows configuration, please refer to the file drivers/pci/fsl_pci_init.c, please refer to int fsl_pci_init_port and fsl_configure_pcie. For the values assignment, please refer to SET_STD_PCIE_INFO section in arch/powerpc/include/asm/fsl_pci.h. So u-boot has completed all required configurations, CodeWarrior could be used to read these registers values.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;In addition, NetComm software(Non OS) based on CodeWarrior including PCIe examples, which could be downloaded from &lt;A class="link-titled" href="http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-tools/suite-for-networked-applications/netcomm-software-resources:NetComm_Software?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1" title="http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-tools/suite-for-networked-applications/netcomm-software-resources:NetComm_Software?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;NetComm Software Resources|NXP&lt;/A&gt; .&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jan 2017 04:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Is-there-a-demo-example-PCIe-setup-in-CodeWarrior-for-the/m-p/618069#M5232</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-01-23T04:11:01Z</dc:date>
    </item>
  </channel>
</rss>