<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: Port pins remains latch at high position when debugger is stopped in Codewarrior</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-pins-remains-latch-at-high-position-when-debugger-is/m-p/616639#M5217</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hemant,&lt;/P&gt;&lt;P&gt;When it run , do not stop, does the PWM can work well ?&lt;/P&gt;&lt;P&gt;You stop the debug, the project stopped, so there is no problem it remains high or low .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 04 Feb 2017 03:41:07 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2017-02-04T03:41:07Z</dc:date>
    <item>
      <title>Port pins remains latch at high position when debugger is stopped in Codewarrior </title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-pins-remains-latch-at-high-position-when-debugger-is/m-p/616638#M5216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using KEA128 and OpenSDA in my project. I am generating PWM signal on port pin. In debug mode if I stop in debug mode, port pin which is generating PWM signal remains in high state. How to fix this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 20:43:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-pins-remains-latch-at-high-position-when-debugger-is/m-p/616638#M5216</guid>
      <dc:creator>hemantsindkar</dc:creator>
      <dc:date>2017-01-13T20:43:49Z</dc:date>
    </item>
    <item>
      <title>Re: Port pins remains latch at high position when debugger is stopped in Codewarrior</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-pins-remains-latch-at-high-position-when-debugger-is/m-p/616639#M5217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hemant,&lt;/P&gt;&lt;P&gt;When it run , do not stop, does the PWM can work well ?&lt;/P&gt;&lt;P&gt;You stop the debug, the project stopped, so there is no problem it remains high or low .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Feb 2017 03:41:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Port-pins-remains-latch-at-high-position-when-debugger-is/m-p/616639#M5217</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-02-04T03:41:07Z</dc:date>
    </item>
  </channel>
</rss>