<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Issues with T4240QDS with RCW BOOT_HO=1 in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Issues-with-T4240QDS-with-RCW-BOOT-HO-1/m-p/615541#M5210</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recently opened a support issue for this and was assigned to Yiping, but for some reason my email responses started bouncing with an automated reply saying send it to &lt;A class="jive-link-email-small" href="mailto:tech.support@nxp.com"&gt;tech.support@nxp.com&lt;/A&gt;, but I used that email, so I am not sure what the issue is. So I am&amp;nbsp;asking here.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a board that we are trying to setup secure boot for, it is a T4240QDS system.&lt;/P&gt;&lt;P&gt;I&amp;nbsp;am currently trying to get the CCS to work with the RCW image BOOT_HO=1, to verify CCS works and BOOT_HO works so I can use it to program the keys for secure boot.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The steps Yiping told me are as follow:&lt;BR /&gt;&lt;SPAN style="font-size: 12pt;"&gt; 1. Please program boot hold off RCW to bank4 RCW address from bank0. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;2. Please power down the target, modify SW6[1-4]=0100 to configure the target to boot from bank4, then power up the target board. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;3. Please open CCS from Start-&amp;gt;All Programs-&amp;gt;Freescale CodeWarrior-&amp;gt;CodeWarrior for PA 10.5.1-&amp;gt;CodeWarrior Connection Server, then type the following commands. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;% delete all&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt; % config cc cwtap:&amp;lt;ip&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt; % ccs::config_chain t4240 &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;% ccs::write_mem 0 0xfe0e00e4 4 0 0x00000001 Then you will see u-boot booting up on bank4.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;I have done the steps 1 and 2 successfully, put the RCW with BOOT_HO=1 to bank4 RCW and set the SW6 switch to boot from the alternative bank. This seems to work because after booting from bank 4, the serial console doesn't output anything, so I assume it is holding until release.&lt;/P&gt;&lt;P&gt;I have some issues with the CCS step however, here are the messages I get from trying to use it&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;CodeWarrior Connection Server console display active (Tcl8.4.12 / Tk8.4.12)&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;Loading CCSAPI Tcl interface (C:/Freescale/CW_PA_v10.5.1/PA/ccs/bin/ccstcl.dll)...&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;Loading Svfburner (C:/Freescale/CW_PA_v10.5.1/PA/ccs/bin/svfburner.dll)...&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;There are no command converters configured&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;Server listening on port: 41475&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;Clients allowed from all hosts&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;No clients denied&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 1 % delete all&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 2 % config cc cwtap:10.15.146.9&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 3 % show cc&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;0: CodeWarrior TAP (cwtap:10.15.146.9) CC software ver. {0.0}&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 4 % ccs::config_chain t4240&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;T4240: HRESET occurred during transaction&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 5 % display ccs::get_config_chain&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;Chain Position 0: T4240&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 6 % ccs::write_mem 0 0xfe0e00e4 4 0 0x0000001&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;HRESET occurred during transaction&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 7 % ccs::write_mem 0 0xfe0e00e4 4 0 0x0000001&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;HRESET occurred during transaction&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 7 %&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px; margin: 0in 0in 0pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;How do I fix this error of "HRESET occurred during transaction"?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Dec 2016 16:45:50 GMT</pubDate>
    <dc:creator>quantran1234</dc:creator>
    <dc:date>2016-12-15T16:45:50Z</dc:date>
    <item>
      <title>Issues with T4240QDS with RCW BOOT_HO=1</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Issues-with-T4240QDS-with-RCW-BOOT-HO-1/m-p/615541#M5210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recently opened a support issue for this and was assigned to Yiping, but for some reason my email responses started bouncing with an automated reply saying send it to &lt;A class="jive-link-email-small" href="mailto:tech.support@nxp.com"&gt;tech.support@nxp.com&lt;/A&gt;, but I used that email, so I am not sure what the issue is. So I am&amp;nbsp;asking here.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a board that we are trying to setup secure boot for, it is a T4240QDS system.&lt;/P&gt;&lt;P&gt;I&amp;nbsp;am currently trying to get the CCS to work with the RCW image BOOT_HO=1, to verify CCS works and BOOT_HO works so I can use it to program the keys for secure boot.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The steps Yiping told me are as follow:&lt;BR /&gt;&lt;SPAN style="font-size: 12pt;"&gt; 1. Please program boot hold off RCW to bank4 RCW address from bank0. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;2. Please power down the target, modify SW6[1-4]=0100 to configure the target to boot from bank4, then power up the target board. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;3. Please open CCS from Start-&amp;gt;All Programs-&amp;gt;Freescale CodeWarrior-&amp;gt;CodeWarrior for PA 10.5.1-&amp;gt;CodeWarrior Connection Server, then type the following commands. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;% delete all&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt; % config cc cwtap:&amp;lt;ip&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt; % ccs::config_chain t4240 &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;% ccs::write_mem 0 0xfe0e00e4 4 0 0x00000001 Then you will see u-boot booting up on bank4.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;I have done the steps 1 and 2 successfully, put the RCW with BOOT_HO=1 to bank4 RCW and set the SW6 switch to boot from the alternative bank. This seems to work because after booting from bank 4, the serial console doesn't output anything, so I assume it is holding until release.&lt;/P&gt;&lt;P&gt;I have some issues with the CCS step however, here are the messages I get from trying to use it&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;CodeWarrior Connection Server console display active (Tcl8.4.12 / Tk8.4.12)&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;Loading CCSAPI Tcl interface (C:/Freescale/CW_PA_v10.5.1/PA/ccs/bin/ccstcl.dll)...&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;Loading Svfburner (C:/Freescale/CW_PA_v10.5.1/PA/ccs/bin/svfburner.dll)...&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;There are no command converters configured&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;Server listening on port: 41475&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;Clients allowed from all hosts&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;No clients denied&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 1 % delete all&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 2 % config cc cwtap:10.15.146.9&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 3 % show cc&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;0: CodeWarrior TAP (cwtap:10.15.146.9) CC software ver. {0.0}&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 4 % ccs::config_chain t4240&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;T4240: HRESET occurred during transaction&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 5 % display ccs::get_config_chain&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;Chain Position 0: T4240&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 6 % ccs::write_mem 0 0xfe0e00e4 4 0 0x0000001&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;HRESET occurred during transaction&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 7 % ccs::write_mem 0 0xfe0e00e4 4 0 0x0000001&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;HRESET occurred during transaction&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;(bin) 7 %&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px; margin: 0in 0in 0pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: 11pt;"&gt;How do I fix this error of "HRESET occurred during transaction"?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 16:45:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Issues-with-T4240QDS-with-RCW-BOOT-HO-1/m-p/615541#M5210</guid>
      <dc:creator>quantran1234</dc:creator>
      <dc:date>2016-12-15T16:45:50Z</dc:date>
    </item>
    <item>
      <title>Re: Issues with T4240QDS with RCW BOOT_HO=1</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Issues-with-T4240QDS-with-RCW-BOOT-HO-1/m-p/615542#M5211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I find a same version T4240QDS board(Sys ID: 0x1e, Sys Ver: 0x14) as yours from our board farm, indeed the rcw 27_55_5_11 cannot work on this version board, please use the attached rcw 1_27_5_11.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please boot the target board at bank0, program rcw to bank4, enter command "qixis_reset altbank"(this command can work at this version board), then open CCS console to type CCS commands. Please refer to the attached u-boot and CCS logs.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 08:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Issues-with-T4240QDS-with-RCW-BOOT-HO-1/m-p/615542#M5211</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-01-13T08:18:40Z</dc:date>
    </item>
  </channel>
</rss>