<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Tools中的主题 Codewarrior 10.7 issue with demo9S08DZ60 eval. board</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-10-7-issue-with-demo9S08DZ60-eval-board/m-p/612249#M5148</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a DELL Vostro PC running windows 7 enterprise service pack 1. &amp;nbsp;Using P&amp;amp;E Hardware Interface Driver, Version 12 (Win XP/Vista/7/8/10) for the USB Multi-link and Codewarrior 10.7. &amp;nbsp;The pre-loaded program that came on the board worked fine. &amp;nbsp;I opened code-warrior and started &amp;nbsp;new bareboard project using absolute assembly. &amp;nbsp;Once the project was created, I entered source.asm and deleted the auto generated stuff. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I then pasted in the supplied example code provided with the board. &amp;nbsp;Before re-flashing an erase-all command was given, which worked, the lights were no longer flashing. &amp;nbsp;Then an erase and flash command was issued. Code warrior said this was completed successfully but the board LEDs are no longer flashing. &amp;nbsp;Please advise. &amp;nbsp;This is for a project-based course at Louisiana State University Shreveport.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Mar 2017 21:05:16 GMT</pubDate>
    <dc:creator>garrettodom</dc:creator>
    <dc:date>2017-03-01T21:05:16Z</dc:date>
    <item>
      <title>Codewarrior 10.7 issue with demo9S08DZ60 eval. board</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-10-7-issue-with-demo9S08DZ60-eval-board/m-p/612249#M5148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a DELL Vostro PC running windows 7 enterprise service pack 1. &amp;nbsp;Using P&amp;amp;E Hardware Interface Driver, Version 12 (Win XP/Vista/7/8/10) for the USB Multi-link and Codewarrior 10.7. &amp;nbsp;The pre-loaded program that came on the board worked fine. &amp;nbsp;I opened code-warrior and started &amp;nbsp;new bareboard project using absolute assembly. &amp;nbsp;Once the project was created, I entered source.asm and deleted the auto generated stuff. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I then pasted in the supplied example code provided with the board. &amp;nbsp;Before re-flashing an erase-all command was given, which worked, the lights were no longer flashing. &amp;nbsp;Then an erase and flash command was issued. Code warrior said this was completed successfully but the board LEDs are no longer flashing. &amp;nbsp;Please advise. &amp;nbsp;This is for a project-based course at Louisiana State University Shreveport.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Mar 2017 21:05:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-10-7-issue-with-demo9S08DZ60-eval-board/m-p/612249#M5148</guid>
      <dc:creator>garrettodom</dc:creator>
      <dc:date>2017-03-01T21:05:16Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10.7 issue with demo9S08DZ60 eval. board</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-10-7-issue-with-demo9S08DZ60-eval-board/m-p/612250#M5149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Garret,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend you to test the mc9s08dz60_demo project that comes with the installation of CodeWarrior, you can find it on the following path:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Freescale\CW MCU v10.7\MCU\CodeWarrior_Examples\HC_Examples\mc9s08dz60_demo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Import this project to your workspace and let me know if it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would also recommend you to create the new project selecting C and ASM languages, this way the startup code will be added to your project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Apr 2017 15:29:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-10-7-issue-with-demo9S08DZ60-eval-board/m-p/612250#M5149</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-04-04T15:29:06Z</dc:date>
    </item>
  </channel>
</rss>