<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Toolsのトピックflash progrramer not programming memory at 0x2180</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/flash-progrramer-not-programming-memory-at-0x2180/m-p/292676#M499</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using code warrior 10.4 for the MC9S08DZ128 microcontroller. When using debug to load my code everything works fine (with the PE Micro USB multilink). If I use the built in flash programmer the memory at 0x2180 and continuing for around 100 bytes does not program. I looked through the various settings but could not find anything that would exclude this area. Anyone run into this?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Nov 2013 20:07:30 GMT</pubDate>
    <dc:creator>martinlockner</dc:creator>
    <dc:date>2013-11-21T20:07:30Z</dc:date>
    <item>
      <title>flash progrramer not programming memory at 0x2180</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/flash-progrramer-not-programming-memory-at-0x2180/m-p/292676#M499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using code warrior 10.4 for the MC9S08DZ128 microcontroller. When using debug to load my code everything works fine (with the PE Micro USB multilink). If I use the built in flash programmer the memory at 0x2180 and continuing for around 100 bytes does not program. I looked through the various settings but could not find anything that would exclude this area. Anyone run into this?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2013 20:07:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/flash-progrramer-not-programming-memory-at-0x2180/m-p/292676#M499</guid>
      <dc:creator>martinlockner</dc:creator>
      <dc:date>2013-11-21T20:07:30Z</dc:date>
    </item>
  </channel>
</rss>