<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックFreescale HCS08 using ROM_8000 as code memory</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Freescale-HCS08-using-ROM-8000-as-code-memory/m-p/597071#M4858</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using freescale microcontroller &lt;STRONG&gt;mc9s08dz96&lt;/STRONG&gt;, CodeWarrior development studio 10.2.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I started facing difficulty to program and debug since project code size has increased beyond 32K. I am using s&lt;STRONG&gt;mall memory model&lt;/STRONG&gt; and till now I was able to keep my code in flash ROM_4000 &amp;amp; ROM_C000. To accommodate some more code I want to use flash&amp;nbsp;ROM_8000 portion of memory.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I tried to use ROM_8000 in small memory model, I faced following issues.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;1. I could not program the .s19 file on target correctly. I am using PE Micro usb multilink interface.&lt;/P&gt;&lt;P&gt;2. I could not debug the code. Due to some problem in copydown segment in startup,c, It was looping&amp;nbsp;back/reseting to start location.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the correct way to use the &lt;STRONG&gt;flash memory ROM_8000&lt;/STRONG&gt; so that I can program and debug project using CodeWarrior studio?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Sep 2016 11:12:25 GMT</pubDate>
    <dc:creator>vikramhande</dc:creator>
    <dc:date>2016-09-07T11:12:25Z</dc:date>
    <item>
      <title>Freescale HCS08 using ROM_8000 as code memory</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Freescale-HCS08-using-ROM-8000-as-code-memory/m-p/597071#M4858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using freescale microcontroller &lt;STRONG&gt;mc9s08dz96&lt;/STRONG&gt;, CodeWarrior development studio 10.2.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I started facing difficulty to program and debug since project code size has increased beyond 32K. I am using s&lt;STRONG&gt;mall memory model&lt;/STRONG&gt; and till now I was able to keep my code in flash ROM_4000 &amp;amp; ROM_C000. To accommodate some more code I want to use flash&amp;nbsp;ROM_8000 portion of memory.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I tried to use ROM_8000 in small memory model, I faced following issues.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;1. I could not program the .s19 file on target correctly. I am using PE Micro usb multilink interface.&lt;/P&gt;&lt;P&gt;2. I could not debug the code. Due to some problem in copydown segment in startup,c, It was looping&amp;nbsp;back/reseting to start location.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the correct way to use the &lt;STRONG&gt;flash memory ROM_8000&lt;/STRONG&gt; so that I can program and debug project using CodeWarrior studio?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Sep 2016 11:12:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Freescale-HCS08-using-ROM-8000-as-code-memory/m-p/597071#M4858</guid>
      <dc:creator>vikramhande</dc:creator>
      <dc:date>2016-09-07T11:12:25Z</dc:date>
    </item>
    <item>
      <title>Re: Freescale HCS08 using ROM_8000 as code memory</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Freescale-HCS08-using-ROM-8000-as-code-memory/m-p/597072#M4859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in 9s08dz96, there are three segments of unbanked Flash ROM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ROM&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; READ_ONLY&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x4000 TO 0x7FFF;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ROM1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; READ_ONLY&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x1900 TO 0x3BFF;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ROM2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; READ_ONLY&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xC000 TO 0xFF7F;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from my understanding, you used ROM and ROM2. do you use ROM1 also?&lt;/P&gt;&lt;P&gt;if not, please also place ROM1 to DEFAULT_ROM.&lt;/P&gt;&lt;P&gt;To use "ROM1,ROM2" as well, pass the option -OnB=b to the compiler&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5150iF5A81396AC7C588D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if all ROM, ROM1 and ROM2 are not enough for you, I suggest you use bank memory mode. because flash memory from 0x8000 is banked memory, we can't use it as unbank.&amp;nbsp; to use flash memory from 0x8000, I suggest you create a new project with wizard with banked memory support, then port your code to the new project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2016 03:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Freescale-HCS08-using-ROM-8000-as-code-memory/m-p/597072#M4859</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-09-08T03:21:10Z</dc:date>
    </item>
  </channel>
</rss>