<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic AN3034SW Error C2801 missing ';' in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/AN3034SW-Error-C2801-missing/m-p/597064#M4856</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to run the sample code from document AN3034 "Using MSCAN on the HCS12 Family". The code is in document AN3034SW. Both of these documents are provided by NXP.&lt;/P&gt;&lt;P&gt;I did modify an include statement and the pragma Link_Info so that it matched the development board I am working with, the MC9S12DG256 development board. &lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to compile the code and I am getting "Error C2801 ';' missing", but it seems like I have all of the appropriate semicolons. It is also strange because the error happens on 4 very similar lines of code. It is during the CANInit function that this occurs. The CANInit function is shown below. The full code is attached. The code that I copied and minimally modified is from AN3034SW. The lines causing errors are in RED. They all cause the same error: "Error C2801 ';' missing". I am using CodeWarrior 5.9.0.&lt;/P&gt;&lt;P&gt;//CANInit Function&lt;/P&gt;&lt;P&gt;void CANInit(void){&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0CTL0 = 0x01;&amp;nbsp; //Enter initialization mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; while(!(CAN0CTL1&amp;amp;0x01)){}; //Wait for initialization mode ACK&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0CTL1 = 0xA0;&amp;nbsp; //Enable MSCAN module and Loopback Mode&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0BTR0 = 0xC7;&amp;nbsp; //Synch Jump = 3Tq clock cycles (re calculate?)&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0BTR1 = 0x3A;&amp;nbsp; //Set number of samples per bit, TSEG1 and TSEG2&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAC = 0x10;&amp;nbsp; //set four 16-bit filters&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; //Acceptance Filters&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR0 = ACC_CODE_ID100_HIGH; //16-bit filter 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN style="color: #e23d39;"&gt;CAN0IDMR0 = MASK_CODE_ST_ID_HIGH; //Accepts Standard Data Frame Msg&amp;nbsp; ERROR Missing ;?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR1 = ACC_CODE_ID100_LOW; //with ID 0x100&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDMR1 = MASK_CODE_ST_ID_LOW;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAC = 0x10; //Not sure why this is twice in code&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR2 = 0x00; //16-bit filter 1&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN style="color: #e23d39;"&gt;CAN0IDMR2 = MASK_CODE_ST_ID_HIGH; //Accepts standard Data frame msg&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR3 = 0x00;&amp;nbsp;&amp;nbsp; //with ID 0x000&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDMR3 = MASK_CODE_ST_ID_LOW;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR4 = 0x00; //16-bit filter 2&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN style="color: #e23d39;"&gt;CAN0IDMR4 = MASK_CODE_ST_ID_HIGH; //Accepts standard Data frame msg&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR5 = 0x00;&amp;nbsp;&amp;nbsp; //with ID 0x000&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDMR5 = MASK_CODE_ST_ID_LOW;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR6 = 0x00; //16-bit filter 3&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN style="color: #e23d39;"&gt;CAN0IDMR6 = MASK_CODE_ST_ID_HIGH; //Accepts standard Data frame msg&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR7 = 0x00;&amp;nbsp;&amp;nbsp; //with ID 0x000&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDMR7 = MASK_CODE_ST_ID_LOW;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0CTL0 = 0x00; //Exit initialization mode request&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; while((CAN0CTL1&amp;amp;0x01)!=0){}; //Wait for normal mode&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;}&amp;nbsp; //end void CANInit&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337857"&gt;main.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 14 Aug 2016 21:10:14 GMT</pubDate>
    <dc:creator>rachelsanford</dc:creator>
    <dc:date>2016-08-14T21:10:14Z</dc:date>
    <item>
      <title>AN3034SW Error C2801 missing ';'</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/AN3034SW-Error-C2801-missing/m-p/597064#M4856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to run the sample code from document AN3034 "Using MSCAN on the HCS12 Family". The code is in document AN3034SW. Both of these documents are provided by NXP.&lt;/P&gt;&lt;P&gt;I did modify an include statement and the pragma Link_Info so that it matched the development board I am working with, the MC9S12DG256 development board. &lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to compile the code and I am getting "Error C2801 ';' missing", but it seems like I have all of the appropriate semicolons. It is also strange because the error happens on 4 very similar lines of code. It is during the CANInit function that this occurs. The CANInit function is shown below. The full code is attached. The code that I copied and minimally modified is from AN3034SW. The lines causing errors are in RED. They all cause the same error: "Error C2801 ';' missing". I am using CodeWarrior 5.9.0.&lt;/P&gt;&lt;P&gt;//CANInit Function&lt;/P&gt;&lt;P&gt;void CANInit(void){&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0CTL0 = 0x01;&amp;nbsp; //Enter initialization mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; while(!(CAN0CTL1&amp;amp;0x01)){}; //Wait for initialization mode ACK&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0CTL1 = 0xA0;&amp;nbsp; //Enable MSCAN module and Loopback Mode&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0BTR0 = 0xC7;&amp;nbsp; //Synch Jump = 3Tq clock cycles (re calculate?)&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0BTR1 = 0x3A;&amp;nbsp; //Set number of samples per bit, TSEG1 and TSEG2&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAC = 0x10;&amp;nbsp; //set four 16-bit filters&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; //Acceptance Filters&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR0 = ACC_CODE_ID100_HIGH; //16-bit filter 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN style="color: #e23d39;"&gt;CAN0IDMR0 = MASK_CODE_ST_ID_HIGH; //Accepts Standard Data Frame Msg&amp;nbsp; ERROR Missing ;?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR1 = ACC_CODE_ID100_LOW; //with ID 0x100&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDMR1 = MASK_CODE_ST_ID_LOW;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAC = 0x10; //Not sure why this is twice in code&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR2 = 0x00; //16-bit filter 1&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN style="color: #e23d39;"&gt;CAN0IDMR2 = MASK_CODE_ST_ID_HIGH; //Accepts standard Data frame msg&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR3 = 0x00;&amp;nbsp;&amp;nbsp; //with ID 0x000&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDMR3 = MASK_CODE_ST_ID_LOW;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR4 = 0x00; //16-bit filter 2&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN style="color: #e23d39;"&gt;CAN0IDMR4 = MASK_CODE_ST_ID_HIGH; //Accepts standard Data frame msg&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR5 = 0x00;&amp;nbsp;&amp;nbsp; //with ID 0x000&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDMR5 = MASK_CODE_ST_ID_LOW;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR6 = 0x00; //16-bit filter 3&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN style="color: #e23d39;"&gt;CAN0IDMR6 = MASK_CODE_ST_ID_HIGH; //Accepts standard Data frame msg&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDAR7 = 0x00;&amp;nbsp;&amp;nbsp; //with ID 0x000&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0IDMR7 = MASK_CODE_ST_ID_LOW;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN0CTL0 = 0x00; //Exit initialization mode request&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; while((CAN0CTL1&amp;amp;0x01)!=0){}; //Wait for normal mode&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;}&amp;nbsp; //end void CANInit&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337857"&gt;main.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 14 Aug 2016 21:10:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/AN3034SW-Error-C2801-missing/m-p/597064#M4856</guid>
      <dc:creator>rachelsanford</dc:creator>
      <dc:date>2016-08-14T21:10:14Z</dc:date>
    </item>
    <item>
      <title>Re: AN3034SW Error C2801 missing ';'</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/AN3034SW-Error-C2801-missing/m-p/597065#M4857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rachel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked your file&amp;nbsp; , there is some spelling error for macro definition .&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1604iB422AC30F438C526/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1645i79FED36E2F63DAEF/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I changed them&amp;nbsp; , please check the attachment .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Aug 2016 06:59:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/AN3034SW-Error-C2801-missing/m-p/597065#M4857</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-08-15T06:59:55Z</dc:date>
    </item>
  </channel>
</rss>