<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic how to add new flash type in CodeWarrior 10.5 in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-add-new-flash-type-in-CodeWarrior-10-5/m-p/584041#M4758</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Customer use 16bit Nand flash(MT29F8G16ADB&lt;STRONG&gt;DA) on bouard, &lt;/STRONG&gt;because with MT29FxG08-IFC.elf(there is only 8 bit algorithm elf in products), failed to read device ID when do programmer on this flash(looks 8 bit algorithm can not be used to access 16 bit device), plan to implement a 16bit algorithm elf file, I found Freescale\CW_PA_v10.5.1\PA\PA_Tools\FlashToolKit\NAND_IFC_Example\ directory, if it can be used as an algorithm template, to go further with this directory, do you&amp;nbsp; have some comments on it?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot for your times!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Aug 2016 13:11:41 GMT</pubDate>
    <dc:creator>liujianbo</dc:creator>
    <dc:date>2016-08-09T13:11:41Z</dc:date>
    <item>
      <title>how to add new flash type in CodeWarrior 10.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-add-new-flash-type-in-CodeWarrior-10-5/m-p/584041#M4758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Customer use 16bit Nand flash(MT29F8G16ADB&lt;STRONG&gt;DA) on bouard, &lt;/STRONG&gt;because with MT29FxG08-IFC.elf(there is only 8 bit algorithm elf in products), failed to read device ID when do programmer on this flash(looks 8 bit algorithm can not be used to access 16 bit device), plan to implement a 16bit algorithm elf file, I found Freescale\CW_PA_v10.5.1\PA\PA_Tools\FlashToolKit\NAND_IFC_Example\ directory, if it can be used as an algorithm template, to go further with this directory, do you&amp;nbsp; have some comments on it?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot for your times!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2016 13:11:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-add-new-flash-type-in-CodeWarrior-10-5/m-p/584041#M4758</guid>
      <dc:creator>liujianbo</dc:creator>
      <dc:date>2016-08-09T13:11:41Z</dc:date>
    </item>
    <item>
      <title>Re: how to add new flash type in CodeWarrior 10.5</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-add-new-flash-type-in-CodeWarrior-10-5/m-p/584042#M4759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN class="replyToName"&gt;Jianbo,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;Yes, this example is designed for users to create a new flash programing algorithm, which is not provided in CodeWarrior. Please import this project in CodeWarrior IDE from File-&amp;gt;Import-&amp;gt;General-&amp;gt;Existing projects into Workspace, edit the the project for your target, and build the project to generate an elf file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;Please refer to C:\Freescale\CW_PA_v10.5.0\PA\PA_Tools\FlashToolKit\Documentation\AppNote-FlashProgrammer-PowerArchitecture.pdf for details, regarding how to add new flash algorithm in CodeWarrior.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;Probably you could configure you target as IFC 8bit NAND mode and try to use MT29FxG08-IFC.elf first.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;Yiping&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Aug 2016 09:37:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-add-new-flash-type-in-CodeWarrior-10-5/m-p/584042#M4759</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2016-08-12T09:37:01Z</dc:date>
    </item>
  </channel>
</rss>