<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Code Warrior and USBDM? in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-Warrior-and-USBDM/m-p/229483#M47</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am very new to "C" programming and the MC9S12XDP512, so please bear with me here. I am working on the Free EMS project that uses this processor on their "Jaguar" engine controller board. I also have a USBDM from "Cool-EFI" that I need to use to load a serial monitor S-19 file into the processor before I can load any operational S-19. I have Code Warrior V 5.9.0, build 5294 installed on my Win 7 machine.&lt;/P&gt;&lt;P&gt;Can I use this version of Code Warrior to load the S-19 and if so, what is the step by step procedure?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Nov 2013 17:00:40 GMT</pubDate>
    <dc:creator>roberthiebert</dc:creator>
    <dc:date>2013-11-26T17:00:40Z</dc:date>
    <item>
      <title>Code Warrior and USBDM?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-Warrior-and-USBDM/m-p/229483#M47</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am very new to "C" programming and the MC9S12XDP512, so please bear with me here. I am working on the Free EMS project that uses this processor on their "Jaguar" engine controller board. I also have a USBDM from "Cool-EFI" that I need to use to load a serial monitor S-19 file into the processor before I can load any operational S-19. I have Code Warrior V 5.9.0, build 5294 installed on my Win 7 machine.&lt;/P&gt;&lt;P&gt;Can I use this version of Code Warrior to load the S-19 and if so, what is the step by step procedure?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2013 17:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-Warrior-and-USBDM/m-p/229483#M47</guid>
      <dc:creator>roberthiebert</dc:creator>
      <dc:date>2013-11-26T17:00:40Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior and USBDM?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-Warrior-and-USBDM/m-p/229484#M48</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we can use hiwave debugger to burn s19 file to flash:&lt;/P&gt;&lt;P&gt;The method is as below:&lt;BR /&gt; 1.&amp;nbsp;&amp;nbsp; Install Codewarrior.&lt;BR /&gt; 2.&amp;nbsp;&amp;nbsp; make sure the hardware is well connected with PC. For instance you are using BDM multilink or Cyclone Pro.&lt;BR /&gt; 3.&amp;nbsp;&amp;nbsp; open Hiwave debugger “Hiwave.exe” in {Your CW install directory}\prog&lt;BR /&gt; 4.&amp;nbsp;&amp;nbsp; then in debugger, go to menu “component”, “set connection…”. In new pop-up small dialog, in the dropdown list, select HC12 and P&amp;amp;E Multilink/Cyclone Pro. Click OK to close this dialog.&lt;BR /&gt; 5.&amp;nbsp;&amp;nbsp; go to menu “MultilinkCyclonePro”, “device”, select the right device chip.&lt;BR /&gt; 6.&amp;nbsp;&amp;nbsp; go to menu “MultilinkCyclonePro”, “connect”, Set the right connection.&lt;BR /&gt; 7.&amp;nbsp;&amp;nbsp; go to menu “File”, “Load application…”. Import the .s19 file into debugger. You could have a browse the content at the memory window of the debugger, it should be in coincidence with the s-record file. &lt;BR /&gt; 8.&amp;nbsp;&amp;nbsp; Press F5 to run. The code should download into the flash.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2013 03:20:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-Warrior-and-USBDM/m-p/229484#M48</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2013-11-27T03:20:01Z</dc:date>
    </item>
  </channel>
</rss>