<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: CodeWarrior 10.6 with MQX 4.0 debugger issue</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572653#M4683</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Vines,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;normally the error message "GDI Protocol fatal error" "The Debugger is not connected to PE device" are not because of the compatibility of CW and MQX version, but a target connection problem.&lt;/P&gt;&lt;P&gt;what debug interface do you work with?&lt;/P&gt;&lt;P&gt;How is the connection work if you create a new project with wizard without MQX support?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Aug 2016 04:02:09 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2016-08-08T04:02:09Z</dc:date>
    <item>
      <title>CodeWarrior 10.6 with MQX 4.0 debugger issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572650#M4680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I recently upgraded my CW software from 10.2 to 10.6. However when I try to debug my application with BSP of MQX 4.0, there was this problem "GDI Protocol fatal error" "The Debugger is not connected to PE device". I am suing PE micro Multilink Universal as my programmer/debugger. I search the forums and I saw a suggestion of updating the driver and then closing CW and re launch with new project workspace. I tried this method but to no avail. I then tried to install MQX 4.2 and debug one of the example programs. I can debug without any problems. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You might asked then just used 4.2 instead? My target platform is Kinetis TWR60d100. And I am still using CW compiler. I have not switch to GNU C Compiler yet. On MQX 4.2 there is no BSP for my target platform. And I am hesitant to convert my application to GNU C as it will cause a ton of problems ( align, etc). &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there anything I need to do to be able to debug under CW 10.6/MQX 4.0? Or is this a limitation like I read on 1 of the questions here in forum about no support for MQX 3.8 in CW 10.6. &lt;/P&gt;&lt;P&gt;FYI&lt;/P&gt;&lt;P&gt;I can see that the chip was programmed correctly, but when I try to break then this dialog box pops out. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Aug 2016 02:54:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572650#M4680</guid>
      <dc:creator>vines</dc:creator>
      <dc:date>2016-08-05T02:54:45Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 10.6 with MQX 4.0 debugger issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572651#M4681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;MQX 3.8 was developed to work with CW MCU v10.1. It is not supported in CW MCU v10.6.&lt;/P&gt;&lt;P&gt; &lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;MQX Task Aware Debugger is integrated with CW MCU v10.6 and is automatically installed. This plug-in can be used with all supported MQX versions (i.e. MQX 4.0.x, MQX 4.1, MQX4.2 and MQX Lite).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Aug 2016 08:11:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572651#M4681</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-08-05T08:11:30Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 10.6 with MQX 4.0 debugger issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572652#M4682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not using 3.8. I just cited it as an example for not being supported in CW 10.6. I am using 4.0 as my MQX. If you could read the first part of my message I mentioned my problems on using 4.0 and CW 10.6 with CW compiler.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2016 02:05:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572652#M4682</guid>
      <dc:creator>vines</dc:creator>
      <dc:date>2016-08-08T02:05:26Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 10.6 with MQX 4.0 debugger issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572653#M4683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Vines,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;normally the error message "GDI Protocol fatal error" "The Debugger is not connected to PE device" are not because of the compatibility of CW and MQX version, but a target connection problem.&lt;/P&gt;&lt;P&gt;what debug interface do you work with?&lt;/P&gt;&lt;P&gt;How is the connection work if you create a new project with wizard without MQX support?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2016 04:02:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572653#M4683</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-08-08T04:02:09Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 10.6 with MQX 4.0 debugger issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572654#M4684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you say connection problem is it the physical connection between programmer to target board? If that is the case, I doubt so. I'll explain why.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I still maintain a CW 10.2 version on my PC. I can debug the same project without an issue using the same PE micro Multilink Universal setup. Then using the same setup, I close CW 10.2 and open my project and try to debug on 10.6 I will have this error. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2016 04:16:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572654#M4684</guid>
      <dc:creator>vines</dc:creator>
      <dc:date>2016-08-08T04:16:04Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 10.6 with MQX 4.0 debugger issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572655#M4685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also after clicking OK in the dialog box &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; font-size: 14px;"&gt;"GDI Protocol fatal error" "The Debugger is not connected to PE device" there is another pop up dialog shown below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; font-size: 14px;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1269iBF09BBC217AB58B1/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; font-size: 14px;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1322i8E7457E363C767B6/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Carlo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2016 04:21:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572655#M4685</guid>
      <dc:creator>vines</dc:creator>
      <dc:date>2016-08-08T04:21:11Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 10.6 with MQX 4.0 debugger issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572656#M4686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anybody out there with similar problems?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 03:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572656#M4686</guid>
      <dc:creator>vines</dc:creator>
      <dc:date>2016-08-10T03:27:54Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 10.6 with MQX 4.0 debugger issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572657#M4687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I ever have similar problem and I fixed the problem by create a new workspace and update the multilink universal driver to the latest.&lt;/P&gt;&lt;P&gt;the driver is included in &lt;STRONG&gt;&lt;SPAN class="font_normal"&gt;&lt;A class="highlight_link" href="http://www.pemicro.com/downloads/download_file.cfm?download_id=346"&gt;USB Multilink Universal (and FX) Resource CD&lt;/A&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/STRONG&gt; from this url&lt;SPAN class="font_micro"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137" title="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137"&gt;P&amp;amp;E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools, debug probes, and …&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there is also a discussion about this problem, can you please check if this can help.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/332909"&gt;GDI Protocol fatal error&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2016 04:13:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-10-6-with-MQX-4-0-debugger-issue/m-p/572657#M4687</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-08-19T04:13:00Z</dc:date>
    </item>
  </channel>
</rss>