<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックMPC5643 generating Two Files each per core??</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MPC5643-generating-Two-Files-each-per-core/m-p/286143#M467</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to know how to generate two ELF each per core under the CodeWarrior? In DPM SRAM has 2 address one is 0x40000000 and 0x50000000 if we use the default project configuration we will see that the project generates code only in 0x40000000 for both cores. How can I make the other code region to be 0x50000000. Also I have another IDEin linux that generates two ELF files can anyone tell me how I can merge them into one?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 05 Jan 2014 03:15:16 GMT</pubDate>
    <dc:creator>tektronix</dc:creator>
    <dc:date>2014-01-05T03:15:16Z</dc:date>
    <item>
      <title>MPC5643 generating Two Files each per core??</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MPC5643-generating-Two-Files-each-per-core/m-p/286143#M467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to know how to generate two ELF each per core under the CodeWarrior? In DPM SRAM has 2 address one is 0x40000000 and 0x50000000 if we use the default project configuration we will see that the project generates code only in 0x40000000 for both cores. How can I make the other code region to be 0x50000000. Also I have another IDEin linux that generates two ELF files can anyone tell me how I can merge them into one?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Jan 2014 03:15:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/MPC5643-generating-Two-Files-each-per-core/m-p/286143#M467</guid>
      <dc:creator>tektronix</dc:creator>
      <dc:date>2014-01-05T03:15:16Z</dc:date>
    </item>
  </channel>
</rss>