<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: CW 6.3 on windows 10</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562616#M4594</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had the same error in the same conditions as you. but i found htat the error only ocurrs when the procesor expert is enabled . When I dont use processor expert , i can open close and work without porblems. For that reason I imagine that the problem is related with the PE. Is any way to reinstall only the PE? best regards Rodrigo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Aug 2016 21:45:26 GMT</pubDate>
    <dc:creator>R_L_</dc:creator>
    <dc:date>2016-08-15T21:45:26Z</dc:date>
    <item>
      <title>CW 6.3 on windows 10</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562607#M4585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to use CW on windows it works fine but when I trie to program an HCS08 micro using the debugger (cyclone pro) it appears " error starting external debugger.Process Error Code 2 (0x02) impossible to find the the specified file "&lt;/P&gt;&lt;P&gt;Can you help me ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jun 2016 14:58:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562607#M4585</guid>
      <dc:creator>azeddinehaida</dc:creator>
      <dc:date>2016-06-23T14:58:35Z</dc:date>
    </item>
    <item>
      <title>Re: CW 6.3 on windows 10</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562608#M4586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CW 6.3 is not recommended for win10. if you need work v6.3 with win10 anyway, try this workaround&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/302974"&gt;Install CodeWarrior 6.3 Windows 7 &amp;amp;amp; 10 x64 directly (Classic version)&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if using win10, NXP's recommendation is CW10.6.4 see this url:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-tools/codewarrior-development-studios/codewarrior-for-microcontrollers/codewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-kinetis-freescale-56xx-rs08-s08-s12z-v10.6:CW-MCU10?code=CW-MCU10&amp;amp;nodeId=015210BAF72726E4C7E4CB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-tools/codewarrior-development-studios/codewarrior-for-microcontrollers/codewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-kinetis-freescale-56xx-rs08-s08-s12z-v10.6:CW-MCU10?code=CW-MCU10&amp;amp;nodeId=015210BAF72726E4C7E4CB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;CodeWarrior for Microcontrollers-Eclipse IDE|NXP&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2016 04:35:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562608#M4586</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-06-24T04:35:46Z</dc:date>
    </item>
    <item>
      <title>Re: CW 6.3 on windows 10</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562609#M4587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;For now I can't change Cw version...Maybe in the future...&lt;/P&gt;&lt;P&gt;But unfortunatly I still having problems ,this time with multiple TARGET and when I close CW.&lt;/P&gt;&lt;P&gt;If I add a new target (cloning an existing target) I can't after select the new targhet ,o moving from to the other.&lt;/P&gt;&lt;P&gt;the same error for both situation is&lt;/P&gt;&lt;P&gt;"CodeWarrior encountered an unhandled exception 0x0eedfade at adress 0x7610dae8&lt;/P&gt;&lt;P&gt;location : KERNELBASE.dll:0x7610dae8&lt;/P&gt;&lt;P&gt;crash dump written to C:\ProgramFiles(x86)\Freescale\codewarrior for Microcontrollers V6.3\bin\IDE.exe.b5292.20160712.103729A.dump "&lt;/P&gt;&lt;P&gt;many thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 09:14:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562609#M4587</guid>
      <dc:creator>azeddinehaida</dc:creator>
      <dc:date>2016-07-12T09:14:14Z</dc:date>
    </item>
    <item>
      <title>Re: CW 6.3 on windows 10</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562610#M4588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;do you&amp;nbsp; use CW6.3 on win10?&lt;/P&gt;&lt;P&gt;you install CW6.3 on win10 directly or use the workaround?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 09:24:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562610#M4588</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-07-12T09:24:11Z</dc:date>
    </item>
    <item>
      <title>Re: CW 6.3 on windows 10</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562611#M4589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Directly.&lt;/P&gt;&lt;P&gt;All is working fine except the two issues above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 09:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562611#M4589</guid>
      <dc:creator>azeddinehaida</dc:creator>
      <dc:date>2016-07-12T09:35:19Z</dc:date>
    </item>
    <item>
      <title>Re: CW 6.3 on windows 10</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562612#M4590</link>
      <description>&lt;P&gt;&lt;A href="https://www.cvorg.ece.udel.edu/2021/03/24/how-to-install-codewarrior-6-3-classic-in-windows-10-or-7-x64/" rel="nofollow noreferrer" target="_blank"&gt;https://www.cvorg.ece.udel.edu/2021/03/24/how-to-install-codewarrior-6-3-classic-in-windows-10-or-7-x64/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This process includes the PE Micro fixes.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Mar 2021 02:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562612#M4590</guid>
      <dc:creator>RodneyMcGee</dc:creator>
      <dc:date>2021-03-31T02:51:49Z</dc:date>
    </item>
    <item>
      <title>Re: CW 6.3 on windows 10</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562613#M4591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I apologize for the delay !!&lt;/P&gt;&lt;P&gt;Strange but true the problem was that the application " HIWAVE.EXE" was not present in the folder \\Prog ,something was wrong with the installation .&lt;/P&gt;&lt;P&gt;The second problems is not solved .&lt;/P&gt;&lt;P&gt;Excuse me for my english is not very good .&lt;/P&gt;&lt;P&gt;When you want to create the abs or abs19 files with different features depending on the define of something you can use different targets &lt;/P&gt;&lt;P&gt;for example&lt;/P&gt;&lt;P&gt;word variable; &lt;/P&gt;&lt;P&gt;if you want to have different version of your abs the first one with&lt;/P&gt;&lt;P&gt;variable = 0x01;&lt;/P&gt;&lt;P&gt;and the second one with&lt;/P&gt;&lt;P&gt;variable= 0x0f ;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can create a new target with an ohter name cloning tha standard target and in the compiler you can define a name as you want for example _BIS_&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in the project you can write &lt;/P&gt;&lt;P&gt;#ifdef _BIS_&lt;/P&gt;&lt;P&gt;variable = 0x0f;&lt;/P&gt;&lt;P&gt;#else&lt;/P&gt;&lt;P&gt;variable = 0x01;&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;P&gt;if you change in the new target in&amp;nbsp; the linker application the name of the abs file ,when you compile the two targets in the BIN folder you will have two 6 files 3 for the standard target and 3 for the clone .&lt;/P&gt;&lt;P&gt;*.abs&lt;/P&gt;&lt;P&gt;*.abs19&lt;/P&gt;&lt;P&gt;*.map&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2016 12:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562613#M4591</guid>
      <dc:creator>azeddinehaida</dc:creator>
      <dc:date>2016-08-09T12:47:39Z</dc:date>
    </item>
    <item>
      <title>Re: CW 6.3 on windows 10</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562614#M4592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;" HIWAVE.EXE" is necessary for the CW install.&amp;nbsp; To guarantee the&amp;nbsp; completeness of the CW6.3 install, I suggest you install your CW6.3 to a 32bit xp/win7 computer then copy the install folder to your disk. then test your connection again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regarding to your second problem, I suggest you read&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-332027"&gt;How to support multiple targets in CodeWarrior(Classic, Eclipse)/KDS&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;chapter 1 is for classic CW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;to switch target, you need click on the red icon in Target tab&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2134iA8446426712BB08B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Aug 2016 07:01:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562614#M4592</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-08-12T07:01:50Z</dc:date>
    </item>
    <item>
      <title>Re: CW 6.3 on windows 10</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562615#M4593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I know very well how is working because I'm using CW 6.3 every day but when I was on xp there wasn't any problems .Now with Windows 10 I'm having this problems (also when I quit from Cw every time crash dump al kernell base).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Aug 2016 08:52:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562615#M4593</guid>
      <dc:creator>azeddinehaida</dc:creator>
      <dc:date>2016-08-12T08:52:20Z</dc:date>
    </item>
    <item>
      <title>Re: CW 6.3 on windows 10</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562616#M4594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had the same error in the same conditions as you. but i found htat the error only ocurrs when the procesor expert is enabled . When I dont use processor expert , i can open close and work without porblems. For that reason I imagine that the problem is related with the PE. Is any way to reinstall only the PE? best regards Rodrigo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Aug 2016 21:45:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562616#M4594</guid>
      <dc:creator>R_L_</dc:creator>
      <dc:date>2016-08-15T21:45:26Z</dc:date>
    </item>
    <item>
      <title>Re: CW 6.3 on windows 10</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562617#M4595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;we can install part of CW feature by custom install. choose custom install, then disable the feature that you needn't install:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2424i26676A64DBD32F01/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CW6.3 is a very old CW product and it isn't designed for win10. NXP doesn't have systemic test of CW6.3 on win10.&lt;/P&gt;&lt;P&gt;so NXP doesn't recommend user uses CW6.3 on win10 and can't provide support of CW6.3 on win10. &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2016 06:35:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562617#M4595</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-08-16T06:35:03Z</dc:date>
    </item>
    <item>
      <title>Re: CW 6.3 on windows 10</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562618#M4596</link>
      <description>&lt;P&gt;I do not recommend removing ProcessorExpert as shown in Jennie's post&amp;nbsp;because:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Processor expert crash issue has been fixed in 6.3, you need to update PE_Plugin.dll&lt;/P&gt;&lt;P&gt;See the new step and download in &amp;nbsp;&lt;A href="https://www.cvorg.ece.udel.edu/2021/03/24/how-to-install-codewarrior-6-3-classic-in-windows-10-or-7-x64/" rel="nofollow noreferrer" target="_blank"&gt;https://www.cvorg.ece.udel.edu/2021/03/24/how-to-install-codewarrior-6-3-classic-in-windows-10-or-7-x64/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Mar 2021 02:48:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CW-6-3-on-windows-10/m-p/562618#M4596</guid>
      <dc:creator>RodneyMcGee</dc:creator>
      <dc:date>2021-03-31T02:48:51Z</dc:date>
    </item>
  </channel>
</rss>