<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックHow to solve the problem of the USB-ML-CFE emulator?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-solve-the-problem-of-the-USB-ML-CFE-emulator/m-p/554225#M4562</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem on the USB-ML-CFE Rev.D&lt;/P&gt;&lt;P&gt;I often use the USB-ML-CFE Rev.D to develop the program on the CPU MCF5484 ,debug the program on line,erase the flash and progam the flash,but now ,I fail to erase and program the flash.&amp;nbsp; The only thing I can do is to debug the program on the line.&amp;nbsp; the MCF5484 module I am using is sured to behave correctly.&lt;/P&gt;&lt;P&gt;Erase operation:&lt;/P&gt;&lt;P&gt;I use the CF FLASHER&amp;nbsp; tool to erase the external flash S29GL128N ,the erase progress reach the end and message shows that&amp;nbsp; the flash has been erased completely .if successed, the memory window ,should be filled with 0xff, but in fact with 0x00,the result is not correct in fact.&lt;/P&gt;&lt;P&gt;Program operation:&lt;/P&gt;&lt;P&gt;I also use the CF FLASHER to program the flash , it seems as the progress has been done completely ,but when I&amp;nbsp; verify this program ,the verifying operation fail.&lt;/P&gt;&lt;P&gt;Debug the program using the CodeWarrior&lt;/P&gt;&lt;P&gt;I write a small pease of program and set the register to switch the led on and off,this program can run correctly as I expected.&lt;/P&gt;&lt;P&gt;So I want to get a help ,who can save me from this problem? thank you in advance. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jun 2016 07:43:01 GMT</pubDate>
    <dc:creator>renrui684</dc:creator>
    <dc:date>2016-06-21T07:43:01Z</dc:date>
    <item>
      <title>How to solve the problem of the USB-ML-CFE emulator?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-solve-the-problem-of-the-USB-ML-CFE-emulator/m-p/554225#M4562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem on the USB-ML-CFE Rev.D&lt;/P&gt;&lt;P&gt;I often use the USB-ML-CFE Rev.D to develop the program on the CPU MCF5484 ,debug the program on line,erase the flash and progam the flash,but now ,I fail to erase and program the flash.&amp;nbsp; The only thing I can do is to debug the program on the line.&amp;nbsp; the MCF5484 module I am using is sured to behave correctly.&lt;/P&gt;&lt;P&gt;Erase operation:&lt;/P&gt;&lt;P&gt;I use the CF FLASHER&amp;nbsp; tool to erase the external flash S29GL128N ,the erase progress reach the end and message shows that&amp;nbsp; the flash has been erased completely .if successed, the memory window ,should be filled with 0xff, but in fact with 0x00,the result is not correct in fact.&lt;/P&gt;&lt;P&gt;Program operation:&lt;/P&gt;&lt;P&gt;I also use the CF FLASHER to program the flash , it seems as the progress has been done completely ,but when I&amp;nbsp; verify this program ,the verifying operation fail.&lt;/P&gt;&lt;P&gt;Debug the program using the CodeWarrior&lt;/P&gt;&lt;P&gt;I write a small pease of program and set the register to switch the led on and off,this program can run correctly as I expected.&lt;/P&gt;&lt;P&gt;So I want to get a help ,who can save me from this problem? thank you in advance. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 07:43:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-solve-the-problem-of-the-USB-ML-CFE-emulator/m-p/554225#M4562</guid>
      <dc:creator>renrui684</dc:creator>
      <dc:date>2016-06-21T07:43:01Z</dc:date>
    </item>
    <item>
      <title>Re: How to solve the problem of the USB-ML-CFE emulator?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-solve-the-problem-of-the-USB-ML-CFE-emulator/m-p/554226#M4563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ren Rui,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you tell us which CodeWarrior version are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Carlos Mendoza&lt;/P&gt;&lt;P&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2016 14:58:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-solve-the-problem-of-the-USB-ML-CFE-emulator/m-p/554226#M4563</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2016-07-01T14:58:44Z</dc:date>
    </item>
  </channel>
</rss>