<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: How to work with release buttons in MQX and PE?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-work-with-release-buttons-in-MQX-and-PE/m-p/551111#M4556</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Norberto ,&lt;/P&gt;&lt;P&gt;It is not from the interrupt to call Task , While&amp;nbsp; it is init interrupt in the TASK .&lt;/P&gt;&lt;P&gt;I recommend you refer to the interrupt demo under MQX:&amp;nbsp; Freescale_MQX_4_2\mqx\examples\&lt;STRONG&gt;isr&lt;/STRONG&gt;\build&lt;/P&gt;&lt;P&gt;There is also PE-mqx demo under CW : CodeWarrior_Examples\Processor_Expert\MQXLite\Kinetis&lt;/P&gt;&lt;P&gt;There is also a GPIO interrupt demo :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/324484"&gt;How to invoke interrupt in GPIO demo project of mqx for more then one time?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The attachment is a guide for create MQXLITE project on CW with PE, it is the same with MQX .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Aug 2016 10:28:47 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2016-08-25T10:28:47Z</dc:date>
    <item>
      <title>How to work with release buttons in MQX and PE?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-work-with-release-buttons-in-MQX-and-PE/m-p/551110#M4555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi!!!&lt;/P&gt;&lt;P&gt;I have some problems to understand how to get an interruption of two release buttons and call a Task to work with the interruption.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I created a GPIO_LDD component with two GPIO Pin in Rising Edge. I used ISR (no DMA).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to know how these interrupts can be linked to the MQX TASKS Template. I created a task with the name "Buttons_task", and this task sends messages to a Main task (Control Task). I need that buttons_task go to the stack when the button is pressed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Aug 2016 22:41:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-work-with-release-buttons-in-MQX-and-PE/m-p/551110#M4555</guid>
      <dc:creator>norbertoj</dc:creator>
      <dc:date>2016-08-22T22:41:11Z</dc:date>
    </item>
    <item>
      <title>Re: How to work with release buttons in MQX and PE?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-work-with-release-buttons-in-MQX-and-PE/m-p/551111#M4556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Norberto ,&lt;/P&gt;&lt;P&gt;It is not from the interrupt to call Task , While&amp;nbsp; it is init interrupt in the TASK .&lt;/P&gt;&lt;P&gt;I recommend you refer to the interrupt demo under MQX:&amp;nbsp; Freescale_MQX_4_2\mqx\examples\&lt;STRONG&gt;isr&lt;/STRONG&gt;\build&lt;/P&gt;&lt;P&gt;There is also PE-mqx demo under CW : CodeWarrior_Examples\Processor_Expert\MQXLite\Kinetis&lt;/P&gt;&lt;P&gt;There is also a GPIO interrupt demo :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/324484"&gt;How to invoke interrupt in GPIO demo project of mqx for more then one time?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The attachment is a guide for create MQXLITE project on CW with PE, it is the same with MQX .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2016 10:28:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-work-with-release-buttons-in-MQX-and-PE/m-p/551111#M4556</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-08-25T10:28:47Z</dc:date>
    </item>
    <item>
      <title>Re: How to work with release buttons in MQX and PE?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-work-with-release-buttons-in-MQX-and-PE/m-p/551112#M4557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you, I could establish the interrupt.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2016 18:05:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-work-with-release-buttons-in-MQX-and-PE/m-p/551112#M4557</guid>
      <dc:creator>norbertoj</dc:creator>
      <dc:date>2016-09-01T18:05:26Z</dc:date>
    </item>
  </channel>
</rss>