<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CCS endianess (LS1021atwr / CWv2016.01) in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCS-endianess-LS1021atwr-CWv2016-01/m-p/510364#M4339</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently toying with ccs from "CodeWarrior Networked Applications Linux Hosted-Offline v2016.01.tar" in order to prepare the secure boot for my LS1021ATWR board. In &lt;A _jive_internal="true" data-containerid="2020" data-containertype="14" data-objectid="329649" data-objecttype="102" href="https://community.nxp.com/docs/DOC-329649"&gt;Secure Boot/Debug Configuration for LS1&lt;/A&gt; in the example to avoid burning the SRKH fuses, it is explained that the values must be swapped before being written in the registers.&lt;/P&gt;&lt;P&gt;Then to release core0, the value 0x01000000 is written in the DCFG_CCSR_BRR register.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I first try to only release core 0 by performing the same write, but nothing happens. However, if I try to write 0x1 instead, the core correctly comes out of reset. It seems the endianess of ccs from the doc is not the same of the one I am using.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Before trying to burn any fuses, I'd like to be sure of the value I need to input in ccs::write_mem command. Can someone clarify the endianess of ccs, or a wait to check it ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 May 2016 10:08:55 GMT</pubDate>
    <dc:creator>vsiles</dc:creator>
    <dc:date>2016-05-09T10:08:55Z</dc:date>
    <item>
      <title>CCS endianess (LS1021atwr / CWv2016.01)</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCS-endianess-LS1021atwr-CWv2016-01/m-p/510364#M4339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently toying with ccs from "CodeWarrior Networked Applications Linux Hosted-Offline v2016.01.tar" in order to prepare the secure boot for my LS1021ATWR board. In &lt;A _jive_internal="true" data-containerid="2020" data-containertype="14" data-objectid="329649" data-objecttype="102" href="https://community.nxp.com/docs/DOC-329649"&gt;Secure Boot/Debug Configuration for LS1&lt;/A&gt; in the example to avoid burning the SRKH fuses, it is explained that the values must be swapped before being written in the registers.&lt;/P&gt;&lt;P&gt;Then to release core0, the value 0x01000000 is written in the DCFG_CCSR_BRR register.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I first try to only release core 0 by performing the same write, but nothing happens. However, if I try to write 0x1 instead, the core correctly comes out of reset. It seems the endianess of ccs from the doc is not the same of the one I am using.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Before trying to burn any fuses, I'd like to be sure of the value I need to input in ccs::write_mem command. Can someone clarify the endianess of ccs, or a wait to check it ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 May 2016 10:08:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCS-endianess-LS1021atwr-CWv2016-01/m-p/510364#M4339</guid>
      <dc:creator>vsiles</dc:creator>
      <dc:date>2016-05-09T10:08:55Z</dc:date>
    </item>
    <item>
      <title>Re: CCS endianess (LS1021atwr / CWv2016.01)</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCS-endianess-LS1021atwr-CWv2016-01/m-p/510365#M4340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Access via cmsisdap it is little-endian, same as using the core.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 May 2016 11:38:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCS-endianess-LS1021atwr-CWv2016-01/m-p/510365#M4340</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2016-05-09T11:38:59Z</dc:date>
    </item>
  </channel>
</rss>